Inquiry about setting W(1280)xH(720) for MIMXRT1170-EVKB in GUI-Guider-1.9.0-GA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Inquiry about setting W(1280)xH(720) for MIMXRT1170-EVKB in GUI-Guider-1.9.0-GA

ソリューションへジャンプ
539件の閲覧回数
jongminiga
Contributor I

When I use the setting for MIMXRT1170-EVKB in GUI-Guider-1.9.0-GA, it always becomes H(1280) and W(720),
and when I set it to W(1280) and H(720) as a user setting, it stops at Creating Project... status.
I want to create a project with W(1280) and H(720) like DigitalCluster Demo.
How can I do it?

0 件の賞賛
返信
1 解決策
494件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @jongminiga,

I have corroborated this behavior on my side. GUI Guider 1.9.0 indeed gets stuck on "Creating Project" status when setting a custom panel of 1280W x 720H. I will report this issue to the GUI Guider team.

That said, this issue is not present on GUI Guider 1.8.1, so please use that instead for now.

BR,
Edwin.

元の投稿で解決策を見る

1 返信
495件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @jongminiga,

I have corroborated this behavior on my side. GUI Guider 1.9.0 indeed gets stuck on "Creating Project" status when setting a custom panel of 1280W x 720H. I will report this issue to the GUI Guider team.

That said, this issue is not present on GUI Guider 1.8.1, so please use that instead for now.

BR,
Edwin.