When I use the setting for MIMXRT1170-EVKB in GUI-Guider-1.9.0-GA, it always becomes H(1280) and W(720),
and when I set it to W(1280) and H(720) as a user setting, it stops at Creating Project... status.
I want to create a project with W(1280) and H(720) like DigitalCluster Demo.
How can I do it?
解決済! 解決策の投稿を見る。
Hi @jongminiga,
I have corroborated this behavior on my side. GUI Guider 1.9.0 indeed gets stuck on "Creating Project" status when setting a custom panel of 1280W x 720H. I will report this issue to the GUI Guider team.
That said, this issue is not present on GUI Guider 1.8.1, so please use that instead for now.
BR,
Edwin.
Hi @jongminiga,
I have corroborated this behavior on my side. GUI Guider 1.9.0 indeed gets stuck on "Creating Project" status when setting a custom panel of 1280W x 720H. I will report this issue to the GUI Guider team.
That said, this issue is not present on GUI Guider 1.8.1, so please use that instead for now.
BR,
Edwin.