Gui Guider v1.8.1 Windows version: wiget Menu display error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Gui Guider v1.8.1 Windows version: wiget Menu display error

2,667 次查看
ChesterLee
Contributor II

I've built a menu, and added some sub-wigets to it, such as Checkbox, Dropdown. In this fig, I added a container with 3 Checkboxes. But it didn't display as what I set. As you can see, in the Gui Guider, it pre-displayed as the left one. However, in the simulator, it ran as the right (which worked as I wished).

WrongDisplayMenuElements.png

Besides, I'm using Gui Guider-1.8.1-GA on Windows 10.

Could you please help me find out what happened to this?

标记 (3)
0 项奖励
回复
9 回复数

2,626 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @ChesterLee 

I try to reproduce this issue.

My GUI GUIDER version is 1.8.1 GA

HangZhang_0-1730974165730.png

But the layout here is the same as the simulator display.

BR

Hang

 

0 项奖励
回复

2,546 次查看
ChesterLee
Contributor II

Hi @Harry_Zhang ,

Tks for your reply.

Besides this wrong display, I got another instance. The figure is shown as below.

ChesterLee_0-1731387974771.png

They are totally different between the UI design screen & the simulator. I set the correct positions of the widgets. However it only displays correctly on the simulator or my MCU device.

Here are some of the widget contents of this screen which may be helpful for you.

ChesterLee_1-1731388273381.png

I'll really appreciate it if you can help me solve this question!

Best Regard,

Chester

0 项奖励
回复

2,530 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @ChesterLee 

Can you share your project with me? You can delete most of the widgets and keep only the widgets in the image. So I can reproduce this problem.

BR

Hang

0 项奖励
回复

2,525 次查看
ChesterLee
Contributor II

Sure, how could I get in touch with you? Email? Its size is about 40 MB.

0 项奖励
回复

2,518 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @ChesterLee 

You can use 7z compression software.

HangZhang_0-1731394332048.png

After compression, transfer the file here.

HangZhang_1-1731394346807.png

BR

Hang

0 项奖励
回复

2,473 次查看
ChesterLee
Contributor II

Hi @Harry_Zhang ,

Here's my export Gui-Guider project. Please check it!

With smile~

Chester

0 项奖励
回复

2,458 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @ChesterLee 

Thank you for your project. I have reproduced this issue and we will strive to resolve it in the next version.

BR

Hang

0 项奖励
回复

2,430 次查看
ChesterLee
Contributor II

Moring @Harry_Zhang ,

Besides, I want to supply some information -- I created this project on Gui Guider v1.8.0. Then after updating the software, I converted the project from v1.8.0 to v1.8.1. Maybe here's the point about the bug.

Hope it'll be helpful to you!

Best wishes

Chester

0 项奖励
回复

2,426 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @ChesterLee 

Thanks for your information.

BR

Hang

0 项奖励
回复