Gui Guider v1.8.1 Windows version: wiget Menu display error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gui Guider v1.8.1 Windows version: wiget Menu display error

4,822 Views
ChesterLee
Contributor II

I've built a menu, and added some sub-wigets to it, such as Checkbox, Dropdown. In this fig, I added a container with 3 Checkboxes. But it didn't display as what I set. As you can see, in the Gui Guider, it pre-displayed as the left one. However, in the simulator, it ran as the right (which worked as I wished).

WrongDisplayMenuElements.png

Besides, I'm using Gui Guider-1.8.1-GA on Windows 10.

Could you please help me find out what happened to this?

Tags (3)
0 Kudos
Reply
9 Replies

4,781 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @ChesterLee 

I try to reproduce this issue.

My GUI GUIDER version is 1.8.1 GA

HangZhang_0-1730974165730.png

But the layout here is the same as the simulator display.

BR

Hang

 

0 Kudos
Reply

4,701 Views
ChesterLee
Contributor II

Hi @Harry_Zhang ,

Tks for your reply.

Besides this wrong display, I got another instance. The figure is shown as below.

ChesterLee_0-1731387974771.png

They are totally different between the UI design screen & the simulator. I set the correct positions of the widgets. However it only displays correctly on the simulator or my MCU device.

Here are some of the widget contents of this screen which may be helpful for you.

ChesterLee_1-1731388273381.png

I'll really appreciate it if you can help me solve this question!

Best Regard,

Chester

0 Kudos
Reply

4,685 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @ChesterLee 

Can you share your project with me? You can delete most of the widgets and keep only the widgets in the image. So I can reproduce this problem.

BR

Hang

0 Kudos
Reply

4,680 Views
ChesterLee
Contributor II

Sure, how could I get in touch with you? Email? Its size is about 40 MB.

0 Kudos
Reply

4,673 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @ChesterLee 

You can use 7z compression software.

HangZhang_0-1731394332048.png

After compression, transfer the file here.

HangZhang_1-1731394346807.png

BR

Hang

0 Kudos
Reply

4,628 Views
ChesterLee
Contributor II

Hi @Harry_Zhang ,

Here's my export Gui-Guider project. Please check it!

With smile~

Chester

0 Kudos
Reply

4,613 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @ChesterLee 

Thank you for your project. I have reproduced this issue and we will strive to resolve it in the next version.

BR

Hang

0 Kudos
Reply

4,585 Views
ChesterLee
Contributor II

Moring @Harry_Zhang ,

Besides, I want to supply some information -- I created this project on Gui Guider v1.8.0. Then after updating the software, I converted the project from v1.8.0 to v1.8.1. Maybe here's the point about the bug.

Hope it'll be helpful to you!

Best wishes

Chester

0 Kudos
Reply

4,581 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @ChesterLee 

Thanks for your information.

BR

Hang

0 Kudos
Reply