GUI Guider bug report

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GUI Guider bug report

ソリューションへジャンプ
9,348件の閲覧回数
art
NXP Employee
NXP Employee

GUI Guider bug report

Hello all,

The customer (original cases #00374019 and #00374024 in SFDC) reports a bugs in
the GUI Guider software. Below is the customer's messages.

"See the attached figure.
When LINE CAP = butt is set in "arc" widgets, the edge display of Active (white) becomes a straight line.
However, the edge display of Backgroud (yellow) remains round. Is this a bug?
* Because the semicircle remains yellow at the start position.
This time, the customer wants to use a straight line both inside and outside the curve.

By the way, the latest version of Gui Guider is 1.1.0.

In the previous 1.0.0, it was a straight line as intended on the GUI, but when it was displayed on the Simulator and the actual board, it became a circle."

"Regarding Gui Guider, if the line is thickened as shown in the attachment, the display will be misaligned on the Simulator and GUI.
Is this a bug?
* The left is the layout on the GUI, and the right is the display on the Simulator.

The customer's environment is as follows.

· MCU to be used

I.MX RT1064

· GUI Guider

Version 1.1.0-GA

· Windows

Windows 10 pro

Version 1909

System type

64-bit operating system, x64-based processor

· MCUXpresso IDE

V11.3.1 [build 5262] [2021-04-02]

· SDK_2x_EVK-MIMRT1064

Version 2.9.2

Manifest Version 3.8.0

So, can someone please check/fix the issues above?

Best Regards,
Artur

ラベル(1)
0 件の賞賛
返信
1 解決策
9,164件の閲覧回数
zhenhualuo
NXP Employee
NXP Employee

The two bugs are fixed in GUI Guider v1.2.0 release, the new version can be downloaded from https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER. 

image.png

 

元の投稿で解決策を見る

2 返答(返信)
9,165件の閲覧回数
zhenhualuo
NXP Employee
NXP Employee

The two bugs are fixed in GUI Guider v1.2.0 release, the new version can be downloaded from https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER. 

image.png

 

9,288件の閲覧回数
zhenhualuo
NXP Employee
NXP Employee

Hi Artur, 

Please see my comments of the 2 issues.

1. “LINE CAP = butt” of arc widget only applies for the edge display of Active part, the edge display of Background doesn’t apply. 

This is a bug of GG, we will fix it in next release, the following line can be added in setup_scr_screen.c to workaround the issue, please replace the first parameter with actual widget name. 

lv_obj_set_style_local_line_rounded(ui->screen_arc_1, LV_ARC_PART_BG, LV_STATE_DEFAULT, 0);

2. When the line is thickened, the display will be misaligned on the Simulator and GUI.

This is a bug of GG, it will be fixed in new GG release. 

 

Best Regards, 

Zhenhua 

0 件の賞賛
返信