GUI Guider bug report

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GUI Guider bug report

Jump to solution
9,635 Views
art
NXP Employee
NXP Employee

GUI Guider bug report

Hello all,

The customer (original cases #00374019 and #00374024 in SFDC) reports a bugs in
the GUI Guider software. Below is the customer's messages.

"See the attached figure.
When LINE CAP = butt is set in "arc" widgets, the edge display of Active (white) becomes a straight line.
However, the edge display of Backgroud (yellow) remains round. Is this a bug?
* Because the semicircle remains yellow at the start position.
This time, the customer wants to use a straight line both inside and outside the curve.

By the way, the latest version of Gui Guider is 1.1.0.

In the previous 1.0.0, it was a straight line as intended on the GUI, but when it was displayed on the Simulator and the actual board, it became a circle."

"Regarding Gui Guider, if the line is thickened as shown in the attachment, the display will be misaligned on the Simulator and GUI.
Is this a bug?
* The left is the layout on the GUI, and the right is the display on the Simulator.

The customer's environment is as follows.

· MCU to be used

I.MX RT1064

· GUI Guider

Version 1.1.0-GA

· Windows

Windows 10 pro

Version 1909

System type

64-bit operating system, x64-based processor

· MCUXpresso IDE

V11.3.1 [build 5262] [2021-04-02]

· SDK_2x_EVK-MIMRT1064

Version 2.9.2

Manifest Version 3.8.0

So, can someone please check/fix the issues above?

Best Regards,
Artur

Labels (1)
0 Kudos
Reply
1 Solution
9,451 Views
zhenhualuo
NXP Employee
NXP Employee

The two bugs are fixed in GUI Guider v1.2.0 release, the new version can be downloaded from https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER. 

image.png

 

View solution in original post

2 Replies
9,451 Views
zhenhualuo
NXP Employee
NXP Employee

The two bugs are fixed in GUI Guider v1.2.0 release, the new version can be downloaded from https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER. 

image.png

 

9,575 Views
zhenhualuo
NXP Employee
NXP Employee

Hi Artur, 

Please see my comments of the 2 issues.

1. “LINE CAP = butt” of arc widget only applies for the edge display of Active part, the edge display of Background doesn’t apply. 

This is a bug of GG, we will fix it in next release, the following line can be added in setup_scr_screen.c to workaround the issue, please replace the first parameter with actual widget name. 

lv_obj_set_style_local_line_rounded(ui->screen_arc_1, LV_ARC_PART_BG, LV_STATE_DEFAULT, 0);

2. When the line is thickened, the display will be misaligned on the Simulator and GUI.

This is a bug of GG, it will be fixed in new GG release. 

 

Best Regards, 

Zhenhua 

0 Kudos
Reply