open the file S32K_PMSM_Sensorless.pmp error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

open the file S32K_PMSM_Sensorless.pmp error

ソリューションへジャンプ
4,874件の閲覧回数
Lilac
Contributor I

when I double click S32k_PMSM_Sensorless.pmp, I can't open the FreeMaster.

It will show like this:

Lilac_0-1638172283601.pngLilac_0-1638172283601.png

which means:The file handle associated with ...... is incorrect.

0 件の賞賛
返信
1 解決策
4,865件の閲覧回数
ArchieLuo
Contributor III

使用3.0版本的FreeMaster打开就可以了。这个应该是新版本创建的(或者是用新版本打开过再保存的),旧版本的FreeMaster打开不了。

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,845件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello,

most probably you have an older version installed and it fails to open a project saved in later version. Updating to the latest (3.1.3) should resolve the issue.

Regards,
Michal

0 件の賞賛
返信
4,866件の閲覧回数
ArchieLuo
Contributor III

使用3.0版本的FreeMaster打开就可以了。这个应该是新版本创建的(或者是用新版本打开过再保存的),旧版本的FreeMaster打开不了。

0 件の賞賛
返信
4,843件の閲覧回数
Lilac
Contributor I

谢谢啦!已解决

0 件の賞賛
返信
4,837件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Please close this thread by marking an answer as "correct" if you consider the issue solved. 

Thanks,
Michal

0 件の賞賛
返信