open the file S32K_PMSM_Sensorless.pmp error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

open the file S32K_PMSM_Sensorless.pmp error

Jump to solution
4,963 Views
Lilac
Contributor I

when I double click S32k_PMSM_Sensorless.pmp, I can't open the FreeMaster.

It will show like this:

Lilac_0-1638172283601.png

which means:The file handle associated with ...... is incorrect.

0 Kudos
Reply
1 Solution
4,954 Views
ArchieLuo
Contributor III

使用3.0版本的FreeMaster打开就可以了。这个应该是新版本创建的(或者是用新版本打开过再保存的),旧版本的FreeMaster打开不了。

View solution in original post

0 Kudos
Reply
4 Replies
4,934 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,

most probably you have an older version installed and it fails to open a project saved in later version. Updating to the latest (3.1.3) should resolve the issue.

Regards,
Michal

0 Kudos
Reply
4,955 Views
ArchieLuo
Contributor III

使用3.0版本的FreeMaster打开就可以了。这个应该是新版本创建的(或者是用新版本打开过再保存的),旧版本的FreeMaster打开不了。

0 Kudos
Reply
4,932 Views
Lilac
Contributor I

谢谢啦!已解决

0 Kudos
Reply
4,926 Views
MichalH
NXP Apps Support
NXP Apps Support

Please close this thread by marking an answer as "correct" if you consider the issue solved. 

Thanks,
Michal

0 Kudos
Reply