can freemaster add a feature that user can process the sample data?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can freemaster add a feature that user can process the sample data?

ソリューションへジャンプ
1,774件の閲覧回数
tiasum
Contributor I

can freemaster add a feature that user can process the sample data in watch table?

for example ,i want to process the p01_out data in the form of p01_out/19200*300

can we add some basic math to help user process the sample data,thx u!

1.png

 

0 件の賞賛
返信
1 解決策
1,759件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

Hi @tiasum,

FreeMASTER supports "Real type transformation". You need to set "Show as" property on your variable to "REAL" to enable it. For more information on this functionality you can refer to Ch. 4.2 Variables (Real type transformation) of the User Manual.

Capture.PNG

 

Hope it helps,
Iulian  

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,760件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

Hi @tiasum,

FreeMASTER supports "Real type transformation". You need to set "Show as" property on your variable to "REAL" to enable it. For more information on this functionality you can refer to Ch. 4.2 Variables (Real type transformation) of the User Manual.

Capture.PNG

 

Hope it helps,
Iulian  

0 件の賞賛
返信