can freemaster add a feature that user can process the sample data?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can freemaster add a feature that user can process the sample data?

Jump to solution
1,751 Views
tiasum
Contributor I

can freemaster add a feature that user can process the sample data in watch table?

for example ,i want to process the p01_out data in the form of p01_out/19200*300

can we add some basic math to help user process the sample data,thx u!

1.png

 

0 Kudos
Reply
1 Solution
1,736 Views
iulian_stan
NXP Employee
NXP Employee

Hi @tiasum,

FreeMASTER supports "Real type transformation". You need to set "Show as" property on your variable to "REAL" to enable it. For more information on this functionality you can refer to Ch. 4.2 Variables (Real type transformation) of the User Manual.

Capture.PNG

 

Hope it helps,
Iulian  

View solution in original post

0 Kudos
Reply
1 Reply
1,737 Views
iulian_stan
NXP Employee
NXP Employee

Hi @tiasum,

FreeMASTER supports "Real type transformation". You need to set "Show as" property on your variable to "REAL" to enable it. For more information on this functionality you can refer to Ch. 4.2 Variables (Real type transformation) of the User Manual.

Capture.PNG

 

Hope it helps,
Iulian  

0 Kudos
Reply