Freemaster Recorder Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freemaster Recorder Error

1,895 Views
osmanyucel
Contributor I

I created a recorder but it does not work. There is an error 0x80000081(invalid command). I added FMSTR_Recorder(0) also.

0 Kudos
Reply
1 Reply

1,873 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello, 

you do not write what communication interface you are using. Please note that Recorder does not run over JTAG and BDM direct memory access.

In case you use UART, CAN, USB-CDC, Ethernet or JTAG PD-BDM or RTT, the recorder should work. Please make sure you have the recorder enabled in freemaster_cfg. by setting FMSTR_USE_RECORDER 1  (or 2, 3, ... depending on number of recorders you need to run simultaneously).

Regards,
Michal 

0 Kudos
Reply