Why are values never displayed in free Master

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why are values never displayed in free Master

ソリューションへジャンプ
3,531件の閲覧回数
stone123
Contributor I

Using DEVKIT-MPC5744P

     I am tyring to connect the development board to the FREE MASTER v2.0 through OSJTAG.The connection mode I chose is as follows:

step one:

01.jpg01.jpg

step two:

02.jpg02.jpg

step three:

03.jpg03.jpg

step four:

04.jpg04.jpg

step five:

06.jpg06.jpg

step six:

07.jpg07.jpg

step seven:

08.jpg08.jpg

       Although the software shows that I am connected, the data cannot be updated. So I'd like to ask, what's wrong with my operation steps? Is the connection mode selected wrong? Can someone show me the correct operation? Thank you.

0 件の賞賛
返信
1 解決策
3,485件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello,
can you try to use the option P&E Nexus/OSBDM PowerPC?

I also recommend to upgrade to the latest FreeMASTER 3.1.3 as available on the nxp.com/freemaster. This version has more recent version of P&E drivers and it may work better in this case.

Regards,
Michal

 

元の投稿で解決策を見る

2 返答(返信)
3,486件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello,
can you try to use the option P&E Nexus/OSBDM PowerPC?

I also recommend to upgrade to the latest FreeMASTER 3.1.3 as available on the nxp.com/freemaster. This version has more recent version of P&E drivers and it may work better in this case.

Regards,
Michal

 

3,470件の閲覧回数
stone123
Contributor I

Thank you very much for your reply!! I've solved the problem. The problem was due to the wrong connection.Your suggestion is very effective.

0 件の賞賛
返信