Why are values never displayed in free Master

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why are values never displayed in free Master

Jump to solution
3,551 Views
stone123
Contributor I

Using DEVKIT-MPC5744P

     I am tyring to connect the development board to the FREE MASTER v2.0 through OSJTAG.The connection mode I chose is as follows:

step one:

01.jpg

step two:

02.jpg

step three:

03.jpg

step four:

04.jpg

step five:

06.jpg

step six:

07.jpg

step seven:

08.jpg

       Although the software shows that I am connected, the data cannot be updated. So I'd like to ask, what's wrong with my operation steps? Is the connection mode selected wrong? Can someone show me the correct operation? Thank you.

0 Kudos
Reply
1 Solution
3,505 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,
can you try to use the option P&E Nexus/OSBDM PowerPC?

I also recommend to upgrade to the latest FreeMASTER 3.1.3 as available on the nxp.com/freemaster. This version has more recent version of P&E drivers and it may work better in this case.

Regards,
Michal

 

View solution in original post

2 Replies
3,506 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,
can you try to use the option P&E Nexus/OSBDM PowerPC?

I also recommend to upgrade to the latest FreeMASTER 3.1.3 as available on the nxp.com/freemaster. This version has more recent version of P&E drivers and it may work better in this case.

Regards,
Michal

 

3,490 Views
stone123
Contributor I

Thank you very much for your reply!! I've solved the problem. The problem was due to the wrong connection.Your suggestion is very effective.

0 Kudos
Reply