Why are values never displayed in free Master

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Why are values never displayed in free Master

跳至解决方案
3,577 次查看
stone123
Contributor I

Using DEVKIT-MPC5744P

     I am tyring to connect the development board to the FREE MASTER v2.0 through OSJTAG.The connection mode I chose is as follows:

step one:

01.jpg

step two:

02.jpg

step three:

03.jpg

step four:

04.jpg

step five:

06.jpg

step six:

07.jpg

step seven:

08.jpg

       Although the software shows that I am connected, the data cannot be updated. So I'd like to ask, what's wrong with my operation steps? Is the connection mode selected wrong? Can someone show me the correct operation? Thank you.

0 项奖励
回复
1 解答
3,531 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello,
can you try to use the option P&E Nexus/OSBDM PowerPC?

I also recommend to upgrade to the latest FreeMASTER 3.1.3 as available on the nxp.com/freemaster. This version has more recent version of P&E drivers and it may work better in this case.

Regards,
Michal

 

在原帖中查看解决方案

2 回复数
3,532 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello,
can you try to use the option P&E Nexus/OSBDM PowerPC?

I also recommend to upgrade to the latest FreeMASTER 3.1.3 as available on the nxp.com/freemaster. This version has more recent version of P&E drivers and it may work better in this case.

Regards,
Michal

 

3,516 次查看
stone123
Contributor I

Thank you very much for your reply!! I've solved the problem. The problem was due to the wrong connection.Your suggestion is very effective.

0 项奖励
回复