When I install version 3.2.6.3 of FreeMaster, I cannot recognize ZLG's CANFD device.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When I install version 3.2.6.3 of FreeMaster, I cannot recognize ZLG's CANFD device.

Jump to solution
3,807 Views
yang_jacky
Contributor III

无法识别ZLG.png

When I install version 3.2.6.3 of FreeMaster, I cannot recognize ZLG's CANFD device. Do I need to install a driver? How to install the driver on my Windows 10 computer?

0 Kudos
Reply
1 Solution
3,736 Views
yang_jacky
Contributor III
HIi, Michal
When I runing the ""rigister.bat", It work! Thank you so much.

View solution in original post

0 Kudos
Reply
7 Replies
3,783 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello, 

there is a new type of ZLG devices which are controlled using ZCANPRO ZCAN library. 

See screenshot:

MichalH_0-1765958509921.png

Regards,
Michal

0 Kudos
Reply
3,779 Views
yang_jacky
Contributor III
The DLL for ZLG has been loaded, but the "CAN Driver" column still displays "ZLG (Driver not loaded)"。And how to solve it?
0 Kudos
Reply
3,772 Views
MichalH
NXP Apps Support
NXP Apps Support

You need to select "ZLG-ZCAN API" in the FreeMASTER (see my screenshot in previous post). And you also need to have ZLG ZCANPRO software installed on your computer. 

Regards,
Michal

0 Kudos
Reply
3,769 Views
yang_jacky
Contributor III
There is no "ZLG-ZCAN API" in the options, only "ZLG (Driver not loaded)", and I confirm that the CANFD driver has been installed
0 Kudos
Reply
3,764 Views
MichalH
NXP Apps Support
NXP Apps Support

It could happen that the 3.2.6 installation has failed to register its new plug-ins and you still access the old ones.

First, go to Help/About menu and check if your version is indeed 3.2.6.3.

If yes, then run the Windows Explorer and find the "c:\NXP\FreeMASTER 3.2\FreeMASTER\register.bat". Run this "as administrator". Then re-start the FreeMASTER app.

 

MichalH_0-1765963811570.png

 

MichalH_2-1765964031886.png

Regards,
Michal

 

0 Kudos
Reply
3,737 Views
yang_jacky
Contributor III
HIi, Michal
When I runing the ""rigister.bat", It work! Thank you so much.
0 Kudos
Reply
3,767 Views
yang_jacky
Contributor III
Do I need to replace the 'focpgi. dll' file?
0 Kudos
Reply