Upgrade issue - IFATAL ERROR - Removing earlier version while upgrading failed.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Upgrade issue - IFATAL ERROR - Removing earlier version while upgrading failed.

ソリューションへジャンプ
3,381件の閲覧回数
matejpacha_Ineltech
Contributor II

Hi,

I just tried an upgrade from previous 3.1 version to the latest, but I'm not successful.

The installation itself is started, then it tries to remove previous version, but that is the point when it fails.

The original folder is empty (seems to be removed), I also cannot see it in the system list of installed apps, but the new installer sees it somehow (probably in registers).

Is there any way to make a clean installation, overriding the registry check? Or which registers should I "remove" before the installation starts?

Thank you,

Best regards,

Matej

0 件の賞賛
返信
1 解決策
3,366件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

Hi @matejpacha_Ineltech,

Could you check this thread.

Hope it helps,
Iulian

元の投稿で解決策を見る

2 返答(返信)
3,358件の閲覧回数
matejpacha_Ineltech
Contributor II

Sorry for duplicated thread, I did search for it and did found nothing like that.

Thanks a lot!

Matej

0 件の賞賛
返信
3,367件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

Hi @matejpacha_Ineltech,

Could you check this thread.

Hope it helps,
Iulian