Scope Trigger Options

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Scope Trigger Options

跳至解决方案
2,539 次查看
kabron1
Contributor I

I see no Trigger options in Scope as e.g. in Segger J-Scope.

Is it possible to add it?

Technically it could not be a problem.

标记 (2)
0 项奖励
回复
1 解答
2,528 次查看
MichalH
NXP Apps Support
NXP Apps Support

Dear Vladimir,

the oscilloscope values are all processed on the PC so adding a condition which would hold the data until a trigger comes is definitely technically possible. And it is actually very good idea, I will add it to the feature request backlog for future versions.

Currently, the triggering is only possible in the Recorder, which runs as a part of FreeMASTER driver on the microcontroller side. You would need to connect using Serial, CAN or packet-driven JTAG/BDM (PD-BDM) option to make use of the Recorder feature.

Thank you,
Michal

 

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,529 次查看
MichalH
NXP Apps Support
NXP Apps Support

Dear Vladimir,

the oscilloscope values are all processed on the PC so adding a condition which would hold the data until a trigger comes is definitely technically possible. And it is actually very good idea, I will add it to the feature request backlog for future versions.

Currently, the triggering is only possible in the Recorder, which runs as a part of FreeMASTER driver on the microcontroller side. You would need to connect using Serial, CAN or packet-driven JTAG/BDM (PD-BDM) option to make use of the Recorder feature.

Thank you,
Michal

 

 

0 项奖励
回复