Scope Trigger Options

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Scope Trigger Options

ソリューションへジャンプ
2,504件の閲覧回数
kabron1
Contributor I

I see no Trigger options in Scope as e.g. in Segger J-Scope.

Is it possible to add it?

Technically it could not be a problem.

タグ(2)
0 件の賞賛
返信
1 解決策
2,493件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Dear Vladimir,

the oscilloscope values are all processed on the PC so adding a condition which would hold the data until a trigger comes is definitely technically possible. And it is actually very good idea, I will add it to the feature request backlog for future versions.

Currently, the triggering is only possible in the Recorder, which runs as a part of FreeMASTER driver on the microcontroller side. You would need to connect using Serial, CAN or packet-driven JTAG/BDM (PD-BDM) option to make use of the Recorder feature.

Thank you,
Michal

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,494件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Dear Vladimir,

the oscilloscope values are all processed on the PC so adding a condition which would hold the data until a trigger comes is definitely technically possible. And it is actually very good idea, I will add it to the feature request backlog for future versions.

Currently, the triggering is only possible in the Recorder, which runs as a part of FreeMASTER driver on the microcontroller side. You would need to connect using Serial, CAN or packet-driven JTAG/BDM (PD-BDM) option to make use of the Recorder feature.

Thank you,
Michal

 

 

0 件の賞賛
返信