S32K_BLDC_Sensorless

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K_BLDC_Sensorless

Jump to solution
5,955 Views
XPQ
Contributor I

Dear sir/madam

I met a problem about Freemaster project 'S32K_BLDC_Sensorless'. It can not generate configuration file correctly . When I click the button, it will not generate configuration file. Please help me.

Thanks

XPQ

ferrmaster.jpg

Tags (1)
0 Kudos
Reply
1 Solution
5,860 Views
marekmusak
NXP Employee
NXP Employee

 

Hello,

1) Open original pmp file outside Design Studio

2) Go to top right hand side corner. Configuration icon will appear as shown below 

marekmusak_0-1626162127711.png

3) Click on it.  Application Setting Page will appear on the screen

4) Click on "Browse Project Directory"

marekmusak_1-1626162211246.png

5)   Click "Yes" to allow ActiveX control and navigate to project destination in Design Studio workspace

 

C: \ ...\ MCSPTE1AK144_BLDC_6Step \ Sources \ Config \

 

6) Once done, click Select. Project path should be like this

Project path: {FM_project_loc}../Sources/Config/

 

7) Click Store Data and Apply

marekmusak_3-1626163033532.png

File generation should work properly.

Regards,

Marek

 

View solution in original post

0 Kudos
Reply
5 Replies
5,887 Views
marekmusak
NXP Employee
NXP Employee

 

Thank you for reaching us !

Please, try this pmp project.

Simply replace original one by new one.

Regards,

Marek

0 Kudos
Reply
5,875 Views
XPQ
Contributor I

Dear sir

 thanks for your reply, the new pmp doesn't work. It not only have the same problem with the old one, but also have a new problem. The new problem is that new pmp have wrong align_current and I can't reset it

Thanks

XPQ

0 Kudos
Reply
5,861 Views
marekmusak
NXP Employee
NXP Employee

 

Hello,

1) Open original pmp file outside Design Studio

2) Go to top right hand side corner. Configuration icon will appear as shown below 

marekmusak_0-1626162127711.png

3) Click on it.  Application Setting Page will appear on the screen

4) Click on "Browse Project Directory"

marekmusak_1-1626162211246.png

5)   Click "Yes" to allow ActiveX control and navigate to project destination in Design Studio workspace

 

C: \ ...\ MCSPTE1AK144_BLDC_6Step \ Sources \ Config \

 

6) Once done, click Select. Project path should be like this

Project path: {FM_project_loc}../Sources/Config/

 

7) Click Store Data and Apply

marekmusak_3-1626163033532.png

File generation should work properly.

Regards,

Marek

 

0 Kudos
Reply
5,927 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,

do you get any error when pressing the "Generate.." button? Is the content of the target file unchanged or does it get corrupted?

Thanks,
Michal

0 Kudos
Reply
5,925 Views
XPQ
Contributor I

Dear sir

yes,the file will not change

Thanks

XPQ

0 Kudos
Reply