S32K_BLDC_Sensorless

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,204件の閲覧回数
XPQ
Contributor I

Dear sir/madam

I met a problem about Freemaster project 'S32K_BLDC_Sensorless'. It can not generate configuration file correctly . When I click the button, it will not generate configuration file. Please help me.

Thanks

XPQ

ferrmaster.jpg

タグ(1)
0 件の賞賛
返信
1 解決策
6,109件の閲覧回数
marekmusak
NXP Employee
NXP Employee

 

Hello,

1) Open original pmp file outside Design Studio

2) Go to top right hand side corner. Configuration icon will appear as shown below 

marekmusak_0-1626162127711.png

3) Click on it.  Application Setting Page will appear on the screen

4) Click on "Browse Project Directory"

marekmusak_1-1626162211246.png

5)   Click "Yes" to allow ActiveX control and navigate to project destination in Design Studio workspace

 

C: \ ...\ MCSPTE1AK144_BLDC_6Step \ Sources \ Config \

 

6) Once done, click Select. Project path should be like this

Project path: {FM_project_loc}../Sources/Config/

 

7) Click Store Data and Apply

marekmusak_3-1626163033532.png

File generation should work properly.

Regards,

Marek

 

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
6,136件の閲覧回数
marekmusak
NXP Employee
NXP Employee

 

Thank you for reaching us !

Please, try this pmp project.

Simply replace original one by new one.

Regards,

Marek

0 件の賞賛
返信
6,124件の閲覧回数
XPQ
Contributor I

Dear sir

 thanks for your reply, the new pmp doesn't work. It not only have the same problem with the old one, but also have a new problem. The new problem is that new pmp have wrong align_current and I can't reset it

Thanks

XPQ

0 件の賞賛
返信
6,109件の閲覧回数
marekmusak
NXP Employee
NXP Employee

 

Hello,

1) Open original pmp file outside Design Studio

2) Go to top right hand side corner. Configuration icon will appear as shown below 

marekmusak_0-1626162127711.png

3) Click on it.  Application Setting Page will appear on the screen

4) Click on "Browse Project Directory"

marekmusak_1-1626162211246.png

5)   Click "Yes" to allow ActiveX control and navigate to project destination in Design Studio workspace

 

C: \ ...\ MCSPTE1AK144_BLDC_6Step \ Sources \ Config \

 

6) Once done, click Select. Project path should be like this

Project path: {FM_project_loc}../Sources/Config/

 

7) Click Store Data and Apply

marekmusak_3-1626163033532.png

File generation should work properly.

Regards,

Marek

 

0 件の賞賛
返信
6,176件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello,

do you get any error when pressing the "Generate.." button? Is the content of the target file unchanged or does it get corrupted?

Thanks,
Michal

0 件の賞賛
返信
6,174件の閲覧回数
XPQ
Contributor I

Dear sir

yes,the file will not change

Thanks

XPQ

0 件の賞賛
返信