Problem installing FreeMASTER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem installing FreeMASTER

3,934 Views
carstengroen
Senior Contributor II

I get an error when trying to install FreeMASTER (Win10). Consulting the logfile:

__________________________________________________________________________

Thu Feb 13 04:48:48 CET 2020

Free Memory: 24383 kB
Total Memory: 35972 kB

java.class.path:
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\InstallerData\IAClasses.zip
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\InstallerData\Execute.zip
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows\InstallerData\Execute.zip
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\InstallerData\Resource1.zip
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows\InstallerData\Resource1.zip
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\InstallerData
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows\InstallerData

ZGUtil.CLASS_PATH:
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\InstallerData\IAClasses.zip
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\InstallerData\Execute.zip
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\InstallerData

sun.boot.class.path:
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows\resource\jre\lib\resources.jar
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows\resource\jre\lib\rt.jar
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows\resource\jre\lib\sunrsasign.jar
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows\resource\jre\lib\jsse.jar
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows\resource\jre\lib\jce.jar
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows\resource\jre\lib\charsets.jar
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows\resource\jre\lib\jfr.jar
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows\resource\jre\classes

java.ext.dirs:
    C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows\resource\jre\lib\ext
    C:\WINDOWS\Sun\Java\lib\ext

java.version                  == 1.8.0_162 (Java 1)
java.vm.name                  == Java HotSpot(TM) Client VM
java.vm.vendor                == Oracle Corporation
java.vm.version               == 25.162-b12
java.vm.specification.name    == Java Virtual Machine Specification
java.vm.specification.vendor  == Oracle Corporation
java.vm.specification.version == 1.8
java.specification.name       == Java Platform API Specification
java.specification.vendor     == Oracle Corporation
java.specification.version    == 1.8
java.vendor                   == Oracle Corporation
java.vendor.url               == http://java.oracle.com/
java.class.version            == 52.0
java.library.path             == C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows\resource\jre\bin;C:\WINDOWS\Sun\Java\bin;C:\WINDOWS\system32;C:\WINDOWS;C:\Program Files\SlickEdit Standard 24.0.0\win\;C:\Program Files (x86)\Intel\Intel(R) Management Engine Components\iCLS\;C:\Program Files\Intel\Intel(R) Management Engine Components\iCLS\;C:\Program Files (x86)\Common Files\Oracle\Java\javapath;C:\ProgramData\Oracle\Java\javapath;C:\WINDOWS\system32;C:\WINDOWS;C:\WINDOWS\System32\Wbem;C:\WINDOWS\System32\WindowsPowerShell\v1.0\;C:\WINDOWS\System32\OpenSSH\;C:\Program Files (x86)\Intel\Intel(R) Management Engine Components\DAL;C:\Program Files\Intel\Intel(R) Management Engine Components\DAL;C:\Program Files\Intel\WiFi\bin\;C:\Program Files\Common Files\Intel\WirelessCommon\;C:\Program Files\010 Editor;C:\Users\Carsten Grøn\.dnx\bin;C:\Program Files\Microsoft DNX\Dnvm\;C:\Program Files\Microsoft SQL Server\130\Tools\Binn\;C:\Program Files (x86)\doxygen\bin;C:\Program Files (x86)\Windows Kits\8.1\Windows Performance Toolkit\;C:\Program Files (x86)\Microsoft SQL Server\90\Tools\binn\;C:\Program Files (x86)\IVI Foundation\VISA\WinNT\Bin\;C:\Program Files\IVI Foundation\VISA\Win64\Bin\;C:\Program Files (x86)\IVI Foundation\VISA\WinNT\Bin;C:\Users\Carsten Grøn\AppData\Local\Microsoft\WindowsApps;.
java.compiler                 == null
java.home                     == C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows\resource\jre
java.io.tmpdir                == C:\Users\CARSTE~1\AppData\Local\Temp\
os.name                       == Microsoft Windows 10 Pro
os.arch                       == x86
os.version                    == 10.0.18363
path.separator                == ;
file.separator                == \
file.encoding                 == Cp1252
user.name                     == Carsten Grøn
user.home                     == C:\Users\Carsten Grøn
user.dir                      == C:\Users\Carsten Grøn\AppData\Local\Temp\I1581608865\Windows
user.language                 == en
user.region                   == null
__________________________________________________________________________

Installed Feature(s) FMSTR, FMSTR Lite of FreeMASTER 3.0

Install Begin: FEBRUARY 13, 2020 4:48:03 PM CET
Install End: FEBRUARY 13, 2020 4:48:41 PM CET

Installed by InstallAnywhere 19.0 Premier Build 5868


User Interactions
-----------------


#Choose Product Features
#-----------------------
CHOSEN_FEATURE_LIST=FMSTR,FMSTR Lite
CHOSEN_INSTALL_FEATURE_LIST=FMSTR,FMSTR Lite
CHOSEN_INSTALL_SET=FMSTR

#Choose Install Folder
#---------------------
USER_INSTALL_DIR=C:\\NXP\\FreeMASTER 3.0

#Choose Shortcut Folder
#----------------------
USER_SHORTCUTS=C:\\Users\\Public\\Desktop

#Install
#-------
-fileOverwrite_C\:\\NXP\\FreeMASTER\ 3.0\\_FreeMASTER_installation\\resource\\iawin32.dll=Yes
-fileOverwrite_C\:\\NXP\\FreeMASTER\ 3.0\\_FreeMASTER_installation\\resource\\win64_32_x64.exe=Yes
-fileOverwrite_C\:\\NXP\\FreeMASTER\ 3.0\\_FreeMASTER_installation\\resource\\remove.exe=Yes
-fileOverwrite_C\:\\NXP\\FreeMASTER\ 3.0\\_FreeMASTER_installation\\resource\\invoker.exe=Yes

Summary
-------

Installation: Unsuccessful.

53 Successes
33 Warnings
1 NonFatalErrors
1 FatalErrors

Action Notes:

None

Install Log Detail:

Check Disk Space:         C:\NXP\FreeMASTER 3.0
                          Status: SUCCESSFUL
                          Additional Notes: NOTE - Required Disk Space:690,412,470 Bytes Free Disk Space:735,479,640,064 Bytes 

Check Disk Space:         C:\NXP\FreeMASTER 3.0
                          Status: SUCCESSFUL
                          Additional Notes: NOTE - Required Disk Space:690,412,470 Bytes Free Disk Space:735,479,640,064 Bytes 

Check Disk Space:         C:\NXP\FreeMASTER 3.0
                          Status: SUCCESSFUL
                          Additional Notes: NOTE - Required Disk Space:690,412,470 Bytes Free Disk Space:735,478,161,408 Bytes 

Install Directory:        C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\
                          Status: SUCCESSFUL
                          Additional Notes: NOTE - Directory already existed

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\vcredist_x86_2012.exe
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\vcredist_x86_2013.exe
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\vcredist_x86_2015.exe
                          Status: SUCCESSFUL

Expand Archive:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\vcredist.zip
                          Status: SUCCESSFUL

Execute Command:          C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\vcredist_x86_2012.exe /quiet
                          Status: SUCCESSFUL

Execute Command:          C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\vcredist_x86_2013.exe /quiet
                          Status: SUCCESSFUL

Execute Command:          C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\vcredist_x86_2015.exe /quiet
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\clljni.dll
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\cllSvrUtility.exe
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\cll_app.dll
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\cll_app_libFNP.dll
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\cll_svr.dll
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\cll_svr_libFNP.dll
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\FnpCommsSoap.dll
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\FNP_Act_Installer.dll
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\clljni.dll
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\cllSvrUtility.exe
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\cll_app.dll
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\cll_app_libFNP.dll
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\cll_svr.dll
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\cll_svr_libFNP.dll
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\FnpCommsSoap.dll
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\FnpCommsSoap.so
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\FNP_Act_Installer.dll
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\libclljni.so
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\libcll_app.so
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\libcll_app_libFNP.so
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\libcll_svr.so
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\libcll_svr_libFNP.so
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\FNPLicensingService\FNPLicensingService
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\install_fnp.sh
                          Status: SUCCESSFUL

Install File:             C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\license.jar
                          Status: SUCCESSFUL

Expand Archive:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\freemaster_license_activation.zip
                          Status: SUCCESSFUL

Execute Command:          java "-Djava.library.path=C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86" -jar "C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\license.jar" install -prod 1.0
                          Status: SUCCESSFUL


Execute Command:          java "-Djava.library.path=C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86" -jar "C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\license.jar" verify -feature Activated -version 1.0 -prod FreeMASTER_Lite_1.0.R
                          Status: SUCCESSFUL


Execute Command:          java "-Djava.library.path=C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86" -jar "C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\license.jar" list
                          Status: SUCCESSFUL


Execute Script/Batch file:   Install 32-bit Flexera service
                          Status: SUCCESSFUL


Install Uninstaller:      FreeMASTER 3.0(Install All Uninstaller Components)
                          Status: SUCCESSFUL

Install Directory:        C:\NXP\FreeMASTER 3.0\_FreeMASTER_installation\resource\
                          Status: SUCCESSFUL

Install File:             C:\NXP\FreeMASTER 3.0\_FreeMASTER_installation\resource\iawin32.dll
                          Status: SUCCESSFUL

Install File:             C:\NXP\FreeMASTER 3.0\_FreeMASTER_installation\resource\win64_32_x64.exe
                          Status: SUCCESSFUL

Install File:             C:\NXP\FreeMASTER 3.0\_FreeMASTER_installation\resource\remove.exe
                          Status: SUCCESSFUL

Install File:             C:\NXP\FreeMASTER 3.0\_FreeMASTER_installation\resource\invoker.exe
                          Status: SUCCESSFUL

Install Directory:        C:\NXP\FreeMASTER 3.0\_FreeMASTER_installation\InstData\
                          Status: SUCCESSFUL

Install Uninstaller:      FreeMASTER 3.0(Install All Uninstaller Components)
                          Status: ERROR
                          Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

Uninstall File:           C:\NXP\FreeMASTER 3.0\_FreeMASTER_installation\Logs\FreeMASTER_3.0_Install_02_13_2020_16_48_26.log
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\vcredist_x86_2012.exe
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\vcredist_x86_2013.exe
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\vcredist_x86_2015.exe
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\clljni.dll
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\cllSvrUtility.exe
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\cll_app.dll
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\cll_app_libFNP.dll
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\cll_svr.dll
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\cll_svr_libFNP.dll
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\FnpCommsSoap.dll
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86\FNP_Act_Installer.dll
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\clljni.dll
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\cllSvrUtility.exe
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\cll_app.dll
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\cll_app_libFNP.dll
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\cll_svr.dll
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\cll_svr_libFNP.dll
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\FnpCommsSoap.dll
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\FnpCommsSoap.so
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\FNP_Act_Installer.dll
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\libclljni.so
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\libcll_app.so
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\libcll_app_libFNP.so
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\libcll_svr.so
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64\libcll_svr_libFNP.so
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\FNPLicensingService\FNPLicensingService
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\install_fnp.sh
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall File:           C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\license.jar
                          Status: WARNING
                          Additional Notes: WARNING - The file does not exist 

Uninstall Folder:         C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\FNPLicensingService
                          Status: WARNING
                          Additional Notes: WARNING - The path does not exist

Uninstall Folder:         C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\x64
                          Status: WARNING
                          Additional Notes: WARNING - The path does not exist

Uninstall Folder:         C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll\i86
                          Status: WARNING
                          Additional Notes: WARNING - The path does not exist

Uninstall Folder:         C:\Users\Carsten Grøn\AppData\Local\Temp\741867.tmp\cll
                          Status: WARNING
                          Additional Notes: WARNING - The path does not exist

Remove Registry Entry:    5 HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Uninstall\null
                          Status: SUCCESSFUL

Error occurred while installing the following Action, hence rolling back the installation....!


Action Name:              Trigger Rollback Action
Action Description:       Trigger Rollback Action


Error Details as below:


This action rolls back the Installation.
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Any idea whats going on ?

(Note, there is a space in the username and a "non ASCII" character)

4 Replies

3,705 Views
iulian_stan
NXP Employee
NXP Employee

Hi carstengroen‌,

Could please confirm if the installer automatically rolls back after license validation ?

If so could you check this post and tell me if that helps.

Kind regards,

Iulian

0 Kudos
Reply

3,705 Views
carstengroen
Senior Contributor II

Iulian,

Yes, the installer rolls back after license validation. Deleting the C:\ProgramData\FLEXNet folder did not change anything.

My log (see above) does also not show the same error as in the post you referred to.

Please note that there is a space in the username and non ASCII letter in the name.

0 Kudos
Reply

3,705 Views
iulian_stan
NXP Employee
NXP Employee

Hi carstengroen‌,

Thanks for trying that one. I was able to reproduce your issue using special characters in user path as per your suggestion. Some processes were failing when invocation path contained special symbols. Using custom temporary directory worked for me.

Capture.PNG

Could you try modifying your temporary folder environment variable. Note the installer uses TMP, not TEMP.

 

Kind regards,

Iulian

3,705 Views
carstengroen
Senior Contributor II

Thanks Iulian,

that did the trick :smileyhappy: 

0 Kudos
Reply