[NTBMS Evaluation Board] Error in FreeMaster java script

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[NTBMS Evaluation Board] Error in FreeMaster java script

2,277 次查看
testyoung
Contributor II

I am using the NTBMS evaluation board.
Use FreeMASTER File provided by NXP.
(File Download Link : https://www.nxp.com/webapp/Download?colCode=NTBMS_SW)

However, when I load the project file, a script error occurs.

Click Yes to the various error messages and run the demo.

The demo program stops shortly after.

I need your help..

testyoung_2-1611221362777.pngtestyoung_2-1611221362777.png

 

URL : https://cdnssl.clicktale.net/ptc/e7591c16-8d10-42bb-8432-c1b5e65a4f66.js

testyoung_1-1611221275532.pngtestyoung_1-1611221275532.png

testyoung_3-1611221565623.pngtestyoung_3-1611221565623.png

 

 

0 项奖励
回复
2 回复数

2,270 次查看
iulian_stan
NXP Employee
NXP Employee

Hi @testyoung,

After running this example on my side (note: I'm not familiar with this application nor BMS systems), I noticed that the first page displayed in FreeMASTER is actually application home page from NXP site. FreeMASTER is not a fully featured web browser, thus some JS scripts are failing, to avoid this behavior I would recommend removing that page:

1. Right click on root element in Project tree, and open properties (it may be a bit annoying because you need first to close those popup errors)

Project tree.pngProject tree.png

2. Clear the  "Description URL" input field (you can open that link in a web browser if you need it)

Prop1.PNGProp1.PNG

3. Confirm the change

Prop 2.PNGProp 2.PNG

Now you should see the BMS application control page. I don't have the setup to confirm the functionality but, after removing the link to NXP site I had no more JS errors.

BMS.PNGBMS.PNG

To persist this change make sure to save the project.

Regards,
Iulian

2,256 次查看
testyoung
Contributor II

Thank you.
The above problem has been resolved.

0 项奖励
回复