FreeMaster3.0 Installation failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeMaster3.0 Installation failed

ソリューションへジャンプ
2,721件の閲覧回数
xgy_upc
Contributor III

The error shown in Figure 1 occurred when I installed Freemaster3.0.How can I solve this problem?

figure1.jpg

0 件の賞賛
返信
1 解決策
2,667件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

Hi,

Before troubleshooting this issue, please note that activation is required only by FreeMASTER Lite component, in case you are using FreeMASTER (main desktop application) just disable Lite feature in component selection step during installation process.

pastedImage_6.png

Troubleshooting:

  • Make sure you have admin rights on your machine, as there may be some settings blocking the communication between your computer and the licensing server (ex: a firewall).
  • In case you cannot run the installer with admin privileges you can try an offline activation. The process is similar to the one described in this post HOWTO: Activate S32 Design Studio. Note that it is not excluded that you may run into into other issues due to limited access rights.

Hope this helps,

Iulian

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,668件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

Hi,

Before troubleshooting this issue, please note that activation is required only by FreeMASTER Lite component, in case you are using FreeMASTER (main desktop application) just disable Lite feature in component selection step during installation process.

pastedImage_6.png

Troubleshooting:

  • Make sure you have admin rights on your machine, as there may be some settings blocking the communication between your computer and the licensing server (ex: a firewall).
  • In case you cannot run the installer with admin privileges you can try an offline activation. The process is similar to the one described in this post HOWTO: Activate S32 Design Studio. Note that it is not excluded that you may run into into other issues due to limited access rights.

Hope this helps,

Iulian

0 件の賞賛
返信