FreeMaster LITE License not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeMaster LITE License not working

Jump to solution
2,824 Views
GabeLogan
Contributor I

Hello, I downloaded freeMaster Lite when I put the license code on the installation I get this error message:

 

software activation code is already used on this station for freemaster_lite 3.2

 

Then the instalation rolls back and doesnt let me install.

 

How to solve this?

 

Thanks 

0 Kudos
Reply
1 Solution
2,794 Views
iulian_stan
NXP Employee
NXP Employee

Hi @GabeLogan,

Could you double check that the activation code is meant for your FreeMASTER Lite version.
Latest version of FreeMASTER Lite is 1.3.

During  the installation process you should be prompted to visit NXP site (the link is also available in the product description in the component selection of the installation process).

Capture1.PNG

 

Capture.PNG

 

You need to access that link only once when installing a newer version of FreeMASTER Lite.
After this is done, you will see your license entitlement next to other product versions:

Capture2.PNG

 

Hope it help,
Iulian

View solution in original post

0 Kudos
Reply
1 Reply
2,795 Views
iulian_stan
NXP Employee
NXP Employee

Hi @GabeLogan,

Could you double check that the activation code is meant for your FreeMASTER Lite version.
Latest version of FreeMASTER Lite is 1.3.

During  the installation process you should be prompted to visit NXP site (the link is also available in the product description in the component selection of the installation process).

Capture1.PNG

 

Capture.PNG

 

You need to access that link only once when installing a newer version of FreeMASTER Lite.
After this is done, you will see your license entitlement next to other product versions:

Capture2.PNG

 

Hope it help,
Iulian

0 Kudos
Reply