FTF 2015 トレーニングプレゼンテーション

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FTF 2015 Training Presentations

ディスカッション

ソート順:
This session explains the many interfaces in the Freescale i.MX 6 series of application processors which make it ideal for automotive applications. 
記事全体を表示
Presented by Istone Presented at DwF Digital Networking Shenzhen - January 28, 2015
記事全体を表示
From head to sole, wearable technology has made the leap from early adoption to becoming a growing market that is on a trajectory to exceed the mobile phone. This session will focus on the broad requirements of wearable devices spanning from bare metal implementations to highly customized versions of Android. This session will give you an overview of the software developer's environment and the different choices that are currently available.
記事全体を表示
PROFIBUS, CAN and RS232 are extensively used in communications networks in factories, buildings, transport infrastructures and monitoring/control equipment in our cities. Ethernet offers higher bandwidth and, in many cases, lowers cost--especially when deployed in daisy-chain topology. Technologies such as EtherCAT, PROFINET and EtherNet/IP are testament to this. In this session, we will explore how QorIQ processor families can help equipment manufacturers span this landscape using a QUICC Engine (QE) controller for UART/Ethernet-based protocol implementation, a Enhanced Triple Speed Ethernet Controller (eTSEC) for intelligent Ethernet classification and 2-port switching, and an eight-port gigabit Ethernet switch for wire-rate switching. Reference design software and hardware files will be available to help you start your own PROFIBUS and PROFINET designs. Presented by Hao Sun Presented at DwF Digital Networking Shenzhen - January 28, 2015 Session ID: APF-IND-T0049
記事全体を表示
In this session, attendees will learn what types of applications can be built on a wearable reference platform for the healthcare and fitness markets. Design challenges and requirements for creating your own designs using WaRP, a wearable reference platform (WaRP), with Kinetis MCUs, i.MX applications processors and Freescale sensors will be discussed.
記事全体を表示
This session will cover how to differentiate and to attach Freescale Power Management solutions to most Freescale MCU and MPUs for complete system enablement in IoT, automotive and multi-market applications. Thanks to a complete MCU tool alignment strategy for industrial applications in Transportation, Energy Management and Building Control segments, we can provide the fastest time to market for your customers. The presentation will include live demonstrations  with analog software drivers that are MCU agnostic, in order to better position Freescale Analog System solutions during your next customer visit.
記事全体を表示
Linux is the state of the art software used to enable Freescale LS102x platforms. Freescale provides a custom SDK and a set of networking software build on top of Linux kernel. In order to improve customer performance, it needs a way to analyze the existing performance of the software and find ways to improve it. CodeWarrior IDE is a development environment targeted to debug and analyze Freescale platforms. Software analysis component from CodeWarrior help Freescale developers to analyze the performance of their code running on Linux on LS102x targets. Using CodeWarrior analysis tools, you are able to trace your system execution at multiple levels: system level, kernel level, and user level. Using CodeWarrior analysis tools, developers are able to easy configure, collect and analyze the trace. Performance profilers are available to show the performance of the analyzed system.
記事全体を表示
Android provides a powerful operating system and development environment that can be used to develop connected IoT products very quickly. It further allows developers build up feature-rich HMI solutions with multi-display capabilities, for example it allows dual full-HD HDMI operation on the DIGI ConnectCore 6 SOM. There is a risk that resulting embedded products are open to external attack or user modification. This presentation will discuss the key components of the Android operating system and show how to implement network-enabled embedded applications based on SE Android (Security Enhancements for Android), a completely open-source project that provides a sandboxed application runtime environment preventing unauthorized modification of devices and/or execution of potentially malicious code.
記事全体を表示
In this session, we will first depict the revolutionary 2X faster go-to-market path to launch a device, then illustrate why MicroEJ for Kinetis helps to reduce the B.O.M cost of our customers. MicroEJ enables IoT innovation, reduces time to prototype and product, and also supports a dynamic Apps go-to-market strategy, by leveraging new capabilities such as ultra-fast simulation, prototyping, as well as product customization after deployment in the field driving larger market share for IoT OEMs.
記事全体を表示
Presented by Bin Zhang, Digi International
記事全体を表示
Learn about the latest MCUs recently added to the Kinetis V series, including the Kinetis KV5x MCU - Freescale's first MCU featuring the ARM Cortex-M7 core.
記事全体を表示
This session will discuss a functional, cost and design cycle analysis of product development using SOMs, WaRP Board, custom board and SCM6D based products. This analysis will focus on several design scenarios facing customers and how each of the 4 solutions discussed compare. Further to the analysis will be discussion on time to market studies as well as software development impacts to product lead time. Following this class, you should be better prepared to utilize Freescale SCM portfolio to get your products to market faster.
記事全体を表示
Enterprise storage solutions from Freescale with high availability in all aspects of the design will be discussed in this session. Dual socket design with redundant chip-to-chip interconnect, over 80G of network connectivity, redundant power, redundant SAS connectivity to HDD's and multiple NVMe SSD's for high IOPs are some of the core features of this storage solution. Ability to offload storage traffic (iSCSI and FCoE), RAID5/6 offload using AltiVec, RDMA across SRIO along with SEC, DCE and PME engines with optional C29x cards makes this an ideal enterprise-class, secure data center storage solution.
記事全体を表示
The standard CAN protocol has been extended into CAN Flexible Data (FD) to provide higher bandwidth while keeping the physical characteristics that have made it the most popular automotive in-vehicle communications protocol . This presentation will provide an overview of the changes to the standard as well as address the challenges faced while rolling out and implementing the technology.
記事全体を表示
The Kinetis family of MCUs is in constant growth and has become the most scalable and wide MCU family in the market based on ARM® Cortex™-M processors. KinetisK series, ARM Cortex-M4 based, is adding new cost-effective devices and memory densities. The Kinetis L family, based on the ARM Cortex M0+ core, grows with more ultra-low power devices. The Kinetis W series offers wireless functionality by integrating class-leading sub-1 GHz and 2.4 GHz RF transceivers. For high accuracy electricity metering and test and measurement applications Kinetis M introduces 24-bit sigma delta ADC and low noise amplifiers on-chip. Kinetis V family offers new Motor Control possibilities starting with low cost ARM Cortex M0+ based devices. But there is more to come! This session offers an overview of the current status of Kinetis families and roadmaps.
記事全体を表示
The D-Bug12XZ firmware combined with the Freescale LFBDMPGMR BDM programmer hardware provides a powerful low-level debugging environment for S12 and S12X MagniV devices. There are times when Electronic Control Modules (ECM) in a car will become inoperative or unresponsive to normal communication channels such as CAN or LIN. The Background Debug Module (BDM) on these devices combined with the D-Bug12XZ  debugger provides the ability to reliably ‘hot-connect’ to the S12 and S12X MagniV devices without resetting or disturbing the running target. Once BDM communications is established with the target, the MCU’s I/O and memory resources can be uploaded for analysis. This session will teach the features and use of these tools to ‘hot connect’ to an unresponsive target MCU with the goal of determining the possible cause of the software and/or hardware failure.
記事全体を表示
How Freescale's RF device portfolio can solve problems for many different industries. The focus on uses outside of the traditional cellular infrastructure and how Freescale devices bring unique capabilities to these application areas that include: Industrial Scientific Medical (ISM) applications, including laser, MRI and heating; Land mobile, including public safety, dispatch and remote monitoring; Avionics, including communication, navigation and radar systems. Presented by Yan Vainter Presented at DwF Tel Aviv - January 27, 2015 Session ID: EUF-IND-T0977
記事全体を表示
In this session, we’ll take a look at how Micron is currently supporting the memory needs (DRAM, NAND, NOR, and SSD) of the automotive, industrial, medical, and military (AIMM) markets. Although memory is changing constantly and faster than ever, Micron understands that the AIMM markets require long product lifetimes as well as specific temperatures and package sizes. Learn more about how Micron is supporting these requirements by keeping a close eye on the latest market trends, technology, and interface roadmaps while offering a Product Longevity Program.
記事全体を表示