FTF 2015 トレーニングプレゼンテーション

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FTF 2015 Training Presentations

ディスカッション

ソート順:
How to develop a proper GUI with FreeMASTER and integrate it to a MCU for development and debugging purposes.  FTF-ACC-F1244
記事全体を表示
The training will focus on the DDR controller used in the i.MX53 and i.MX6 series processors. It will include operation, register programming and calibration techniques to properly tune the various DDR types supported: LPDDR2, DDR2 and DDR3. Hardware layout considerations will also be discussed. Presented by Mark Middleton Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-DES-T1060
記事全体を表示
There are many stakeholders in the development of cyber security for the automotive market ranging from car makers, Tier 1/Tier 2 suppliers, service providers, governments, and consumers. This leads to wide variety of requirements, market drivers, and use cases for automotive cyber security. This session will give an overview of these with a focus on the relationship between safety and security, the emerging SAE J3061 recommended practice, and the tradeoffs involved in implementing security features in the automobile. Sample cyber security both from Freescale and 3rd-party software providers will also be described.
記事全体を表示
Kinetis M series microcontrollers integrate high-accuracy measurement units (24-bit SD ADC, PGA, VREF) to measure wide dynamic range analog signals with a very low temperature drift.
記事全体を表示
Beginning 2016, the European New Car Assessment program (NCAP) will allocate increased scoring measures for pedestrian detection capabilities. This means that any car fitted with technologies that enable detection of a pedestrian in a hazardous situation and as a result perform collision avoidance measures shall be rewarded with an increased NCAP score. These systems must be designed and manufactured based on a solid automotive development flow. This session will address the vision processing requirements for pedestrian detection and provide training on how vision algorithms may be implemented to respond to NCAP requirements in a safe, secure and reliable way.
記事全体を表示
This session will provide an opportunity to view a demo with the QorIQ LS1021A Tower board. We will go over using CodeWarrior for Digital Networking ARM®-based products, learn how to use the Processor Expert for QCS tool to generate RCW, how to load up uboot and RCW to the Tower board, and gain experience with the SDK. 
記事全体を表示
As geometries continue to shrink and switching speeds increase, designing electromagnetic systems and printed circuit boards to meet the required signal integrity and EMC specifications has become even more challenging. A new design methodology is required, specifically, the utilization of an electromagnetic physics-based design methodology to control the field energy in your design. This session will walk through the development process and provide guidelines for building successful printed circuited boards.
記事全体を表示
The Kinetis software development kit (SDK) provides a comprehensive software framework for Kinetis MCU-based applications. Join this session to get hands-on experience with the basics of Kinetis SDK, including MCU boot-up, board setup, interrupt handling, HAL and drivers.
記事全体を表示
Learn about the latest MCUs recently added to the Kinetis V series, including the Kinetis KV5x MCU - Freescale's first MCU featuring the ARM Cortex-M7 core.
記事全体を表示
This session provides an overview of our automotive general purpose roadmap, with microcontroller products ranging from 8KB of flash up to 2MB of flash. Come learn about our line of new ARM® Cortex®-M microcontrollers that address general purpose and low-end automotive body applications, and also our line of highly integrated mixed-signal MCUs, combining a microcontroller and high-voltage analog components in a single piece of silicon to address LIN/CAN nodes in space-constrained applications, with optional motor-control pre-drivers. 
記事全体を表示
Learn the major components of an Automotive Traction Inverter by walking through a prototype hardware and software design. I will be highlighting our IGBTs, GDICs, micros, and voltage / frequency (V/F) software to control an induction motor. This class provides a solid foundation on motor control and inverter design and an excellent class for engineers that are involved with EV systems but not yet motor control experts.
記事全体を表示
How to develop a proper GUI with FreeMASTER and integrate it to a MCU for development and debugging purposes.
記事全体を表示
This session will discuss the challenges of supporting multiple execution environments on embedded systems and advocate heterogeneous multiprocessing (HMP) as an effective solution to those challenges. The i.MX architecture will evolve to support HMP based on the integration of ARM Cortex-A and Cortex-M processors into a single SoC. This session will introduce the HMP architectural features available on next-gen i.MX designs, including resource sharing/isolation, interprocessor communication and interprocessor synchronization. Presented by Rob Cosaro Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SHB-T1036
記事全体を表示
This session provides an overview on the security technologies Freescale offers to secure a system through two complementary technologies: 1) the Trust Architecture already present in QorIQ P and T series including Secure Boot and 2) the TrustZone® technology introduced in the ARM®-based QorIQ LS series processors. We will outline the motivations for offering these technologies in embedded processors and show how they can be complementary for making a final system “Trustable” in the sense it does what its users and suppliers expect it to do. 
記事全体を表示
This session will give you an understanding of how power is dissipated in a motor driver. You will also get a hands-on demonstration showing the waveforms of the MC33926 and MC33HB2001 as they are driven into current limit.
記事全体を表示
High-level training session designed to enlighten first-time users of i.MX applications processors with three critical hardware design areas: DRAM Interface Register settings, Major Processor Power Rail Treatment, and high-speed signal layout. Available Freescale resources designed to help customers in these areas will be highlighted.
記事全体を表示
A guide to using the Manufacturing tool. Learn how to install and use the Manufacturing tool on Freescale reference boards and modify the tool for use in your own application.
記事全体を表示
This presentation will highlight the key lessons learned of these deployments and how today's designs need to be architectured to be prepared to this massive innovation wave seen in the metering space including wide variety of markets requirements, wide variety of networks topologies, wide variety of communications protocols and silicon innovation acceleration. The presentation will also review how Freescale has developed a complete strategy around its Kinetis product line that will enable customers to quickly start their designs with low risk, high flexibility and security while being at the optimum price point. 
記事全体を表示