AN12149 IEEE 1588 sync not working well

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN12149 IEEE 1588 sync not working well

1,848件の閲覧回数
ypearson-bdai
Contributor I

Hello

Board: MIMXRT1020-EVK (2 boards connected by patch ethernet cable)

Software: AN12149SW

1 configurated at Master

1 configured as Slave

Oscilloscope connected to J19-10 to observe PPS signal

Issue: PPS pulse will on occasion be ~50ns between master/slave device but after some time will lose sync and be off by ~500us and never recover. Resetting the board may temporarily fix the issue but drift /error will eventually come back.

 

I would like to see if there is a fix to maintain sync between master and slave device

 

 

 

0 件の賞賛
返信
1 返信

1,789件の閲覧回数
daweiyou
NXP Employee
NXP Employee

Try to modify DEFAULT_PDELAYREQ_INTERVAL, DEFAULT_SYNC_INTERVAL, AP, AI

 

daweiyou_0-1708480404937.png

 

0 件の賞賛
返信