Programming FMUK66 for first use

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Programming FMUK66 for first use

跳至解决方案
4,689 次查看
ArifKamal
Contributor I

My RDDRONE-FMUK66 board could not connect using the debugger given by the it. As i was following the gitbook step by step, im stuck at the bootloader part. When using Jlink Commander in Windows and trying to connect MK66FN2M0xxx18 through SWD as the target interface, it gives out a response "cannot connect to target" why is that? can anybody help me?

Screenshot 2021-06-10 040949.png

 

0 项奖励
回复
1 解答
4,676 次查看
dk7xe
Contributor II

You need to power up the FMU via USB or the included power module to be able to program it.

在原帖中查看解决方案

2 回复数
4,677 次查看
dk7xe
Contributor II

You need to power up the FMU via USB or the included power module to be able to program it.

4,666 次查看
ArifKamal
Contributor I

Thank you very much

0 项奖励
回复