Programming FMUK66 for first use

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming FMUK66 for first use

Jump to solution
4,633 Views
ArifKamal
Contributor I

My RDDRONE-FMUK66 board could not connect using the debugger given by the it. As i was following the gitbook step by step, im stuck at the bootloader part. When using Jlink Commander in Windows and trying to connect MK66FN2M0xxx18 through SWD as the target interface, it gives out a response "cannot connect to target" why is that? can anybody help me?

Screenshot 2021-06-10 040949.pngScreenshot 2021-06-10 040949.png

0 Kudos
Reply
1 Solution
4,620 Views
dk7xe
Contributor II

You need to power up the FMU via USB or the included power module to be able to program it.

View solution in original post

2 Replies
4,621 Views
dk7xe
Contributor II

You need to power up the FMU via USB or the included power module to be able to program it.

4,610 Views
ArifKamal
Contributor I

Thank you very much

0 Kudos
Reply