what's the logic_zero or logic_one mean in ADC trigger B input?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

what's the logic_zero or logic_one mean in ADC trigger B input?

跳至解决方案
2,254 次查看
terrybogard
Contributor II

terrybogard_0-1616059512157.png

what's the logic_zero or logic_one mean in ADC trigger B input?

MC56F82746

Processor Expert

标记 (2)
0 项奖励
回复
1 解答
2,230 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Terry,

I think you misunderstood it.

From crossbar hardware perspective, the ADC trigger signal A/B can select any signal from the Table 3-6. XBARA  Inputs, so logic_zero or logic_one are only option, but it does not mean that you can select logic_zero or logic_one to trigger ADC. You can select PWMx_TRG0 or TAx_out signals whatever, it is dependent on your application.

BR

XiangJun Rong

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,237 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Terry,

Pls refer to the Table, the ADC  Trigger A/B signal must be selected from the following table, if you select the XBAR_IN0, it is VSS, it is logic_zero. If you select the XBAR_IN1, it is VDD, it is logic_1. If you select XBAR_IN2, the ADC trigger signal will be from external pad called XB_IN2.

Hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1616121900263.png

 

0 项奖励
回复
2,233 次查看
terrybogard
Contributor II

hi rongjun,

could you pls answer again about how the adc trigger will happen if the logic zero or one is chosen. your previous answer was about how to configure the trigger input to logic zero or one, which is not my wanted answer. such as if logic zero is chosen, adc will never be triggered, or adc will be triggered for all the time if logic one is chosen.

thanks.

0 项奖励
回复
2,231 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Terry,

I think you misunderstood it.

From crossbar hardware perspective, the ADC trigger signal A/B can select any signal from the Table 3-6. XBARA  Inputs, so logic_zero or logic_one are only option, but it does not mean that you can select logic_zero or logic_one to trigger ADC. You can select PWMx_TRG0 or TAx_out signals whatever, it is dependent on your application.

BR

XiangJun Rong

0 项奖励
回复
2,222 次查看
terrybogard
Contributor II

thanks for xiangjun's explain with patience. so it seems make no sense to set the trigger input connect with logic zero or one, and I suggest NXP cancel these two items in menu to avoid misunderstanding.

0 项奖励
回复