Write endurance for the MC56F847XX Program Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Write endurance for the MC56F847XX Program Flash

2,203件の閲覧回数
EngHuiPeng
NXP Employee
NXP Employee

What is the  write endurance for the MC56F847XX Program Flash? Is it 10K cycles? Is there any register that could read on the no. of write cycles. Thanks.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,919件の閲覧回数
EngHuiPeng
NXP Employee
NXP Employee

XiangJun,

Do we have any application examples that Customer could push to the max of the write/read to do testing on their reliability?

Thanks.

Regards,

Audrey

0 件の賞賛
返信

1,920件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Audrey,

The reliability specs of flash in data sheet is provided by test team, as AE engineers, we do not have the test code to test the max of reading and writting.

sorry for not helping you.

BR

Xiangjun Rong

0 件の賞賛
返信

1,920件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

HI,

The minimum cycles of erasing and programming for MC56F847xx flash is 10K, the maximum is 50K.

I copy the specs from the data sheets:

Hope it can help you.

BR

XiangJun Rong

pastedImage_0.png

0 件の賞賛
返信