P1011NXN2DFB Specification Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1011NXN2DFB Specification Question

1,593件の閲覧回数
dannydeng
Contributor III

Can anybody provide the  Max stress  of the IC that could withstand and the Max weight the IC could withstand ?

Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,410件の閲覧回数
LPP
NXP Employee
NXP Employee

Please, refer to AN4259 Section 27.2 Thermal Management for WB-TePBGA

"The heat sink should be attached to the printed-circuit board with the spring force centered over the center of the package. This spring force should not exceed 10 pounds of force (45 Newton)."

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-powe...

0 件の賞賛
返信