Splitter IC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Splitter IC

3,710 Views
Pınar
Contributor I

Hello,

Do you have an IC that can output 1 HDMI input as 2 HDMI outputs (min 4K with HDCP support) at the same time (both outputs active at the same time)? The output should be able to run two different brands and models of monitors at the same time.

Which of your products can we use?

Best Regards;

0 Kudos
Reply
3 Replies

3,690 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please double check whether CBTL06DP213 multiplexing meet your requirement or not.

 

0 Kudos
Reply

3,683 Views
Pınar
Contributor I

Hi there;

If I'm not misinterpreting the datasheet; It is emphasized that only one channel can be selected. We need two active outputs that can output simultaneously.

For example, the circuit whose picture I have attached/shared below provides output to both a 4K HDMI 2.0 (with HDCP) monitor and a VGA monitor at the same time.

We are designing a similar device. Both monitors must be turned on.

We are looking for an IC that can send images to both devices.

Tags (1)
0 Kudos
Reply

3,676 Views
guoweisun
NXP TechSupport
NXP TechSupport

Seems no suitable part!

0 Kudos
Reply