Rewrite software for board 56F8014 digital signal controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Rewrite software for board 56F8014 digital signal controller

17,660件の閲覧回数
mademusa
Contributor I

DEMO56F8014: Demonstration Board for 56F8014 Digital Signal Controller
https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digit...

Hi, I have several mal functioning power supplies for special hardware that have the digital controller 56F8014, I have
run some tests while reparing some of them I realized the controller went corrupt, when moving the chip to a working
power supply it started to show the exact same behaviour. I´d like to know if with the "DEMO56F8014 Demonstration Board
for 56F8014 Digital Signal Controller" Kit I will be able to download the software from a good chip and then write it
the defective ones. Is this possible?

0 件の賞賛
返信
14 返答(返信)

17,639件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suggest you download a evaluation version of CodeWarrior for MCU ver11.x tools from the link:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-l...

You can use USBTAP to download code to on-chip flash of 56F8014 Demo board with 9V DC power supply under Win10 or low version Windows OS.

If you use the classic CodeWarrior for DSP56800E ver8.3, it may have issue under Win10.

Pls try to use CodeWarrior for MCU tools plus USBTAP device and download application code.

BR

XiangJun Rong

 

0 件の賞賛
返信

17,619件の閲覧回数
mademusa
Contributor I

Hi, I have not bought any of the required equipment. I want to know before buying the items, so, are you suggesting i buy the following items?:

DEMO56F8014: Demonstration Board for 56F8014 Digital Signal Controller
https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digit...

and

USBTAP_DSC: USB TAP for ONCE DSC
https://www.nxp.com/design/software/development-software/codewarrior-development-tools/run-control-d...

Also, the software in the working chips is really difficult to find online, so I need the two operations, get the software from a working chip and inject the software to the difective ones.

If this is correct, please let me know so I can buy both items and download the recommended software.

 

0 件の賞賛
返信

17,600件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The MC56F8014 is a bit old, I suggest you order the latest DSC family, for example MC56F83xxx, MC56F81xxx, or MC56F84xxx, MC56F82xxx, among them, the MC56F83xxx, MC56F81xxx are latest families:

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digit...

For example, I suggest you order Development Board for MC56F83xxx Digital Signal Controllers from the link:

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digit...

 

You can order the third party Multilink Universal device so that you can download code when you design your own PCB.

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/universal-mu...

The tools is CodeWarrior for mcu:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-l...

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信

17,588件の閲覧回数
mademusa
Contributor I

Okey, I am going to follow your suggestions.

So, to make sure, do I have to buy 2 separate things?

this https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digit...

and this https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/universal-mu...

and will be able to copy the firmware in a working 56F8014 chip in a power supply and download it to a corrupted chip in another power supply????

 

I can not find the buy button on the second product.

0 件の賞賛
返信

17,586件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the multiLink Universal device, you can order from PEMicro with www.pemicro.com

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320180&productTab=1

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

17,280件の閲覧回数
mademusa
Contributor I

Hello, I just got the product you have recommended me!

The USB Multilink Universal.

To my surprise, none of the connectors matches the board I intend to flash.

I had sent you the pictures before, so I thought one of the cables would match.

Do I have to solder pins to the board to use the 7 pins connector? what would be de possition of the pins?

 

IMG_20220314_184810.jpgIMG_20220314_184810.jpgIMG_20220314_184821.jpgIMG_20220314_184821.jpgIMG_20220314_184829.jpgIMG_20220314_184829.jpgIMG_20220314_184950.jpgIMG_20220314_184950.jpgIMG_20220314_185033.jpgIMG_20220314_185033.jpg

0 件の賞賛
返信

17,252件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

It appears that the MC56F8014 Demo board is incorrect, pls check the processor on the board, is it MC56F8014? BTW, I attach the UM of MC56F8014 Demo board.

BR

XiangJun Rong

0 件の賞賛
返信

17,184件の閲覧回数
mademusa
Contributor I

Thank you for your patience!

The chip number is exacly MC56F8014

I could not get a clear picture, but i can assure you it´s MC56F8014.

If you look at the pictures you can confirm the chip number.

Also since none the cables seemed to match the board, I remove the plastic cover on one of the sides and saw a series of pins that match the number of pins from one of the cables, so i made a adapter myselft, one of the pins on the board is visibly larger the the other ones, so I assumed it`s for the red wire. I have not run any test because I want to wait for your answer to see if its possible.

 

Original BoardOriginal BoardOncovered pins, the one on the left is longer than the other onesOncovered pins, the one on the left is longer than the other onesChip Close UpChip Close UpAdapter I CreatedAdapter I Created

 

0 件の賞賛
返信

17,181件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

This is the picture of the Freescale MC56F8014 Demo board, obviously, it is different from yours.

For your board, I have not your board schematics, pls find out the JTAG pin, and connect with your Multilink Universal device.

BR

XiangJun Rong

xiangjun_rong_0-1648002054134.pngxiangjun_rong_0-1648002054134.png

 

0 件の賞賛
返信

17,172件の閲覧回数
mademusa
Contributor I

Ok, i got it all wrong from the begennig then.

My board is not a demostration board. It`s a board taken from an ELTEK industrial power supply. I repair this kind of power supplies. Now, I have many power supplies of this kind with what I suspect is corrupted MC56F8014 that causes de power supply to work erratically, I know this, because if I swap the board containing the MC56F8014 with the same board on a working power supply, the problems gets solved in the first one and the other one gets the errors.

What I want to be able to do is to extract the software in the chip MC56F8014 on a working board, and write it to an empy chip.

I am not trying to write a new program or anything like that, just reflash the corrupted chips or flash new chips and solder them into the boards.

 

 

 

0 件の賞賛
返信

11,113件の閲覧回数
CrisMa
Contributor I

Hello MADEMUSA,

We can collaborate on this topic. Email me at [email protected]

0 件の賞賛
返信

15,324件の閲覧回数
Terryprieto
Contributor I

Hola MAdemusa, soy de Colombia, también reparo equipos eltek, quizás nos podamos colaborar, escríbeme!!!

タグ(1)
0 件の賞賛
返信

11,111件の閲覧回数
CrisMa
Contributor I

Hola Terry,

¿Podemos colaborar en este tema? Me dejas tu mail o puedes escribir al mail [email protected]

0 件の賞賛
返信

15,504件の閲覧回数
danieltepuy
Contributor I

Hi Mademusa.

Did you manage to get a way to read and write this card?

 

0 件の賞賛
返信