About NCJ29D6 chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About NCJ29D6 chip

3,025 Views
BrianYeh
Contributor I

Dear NXP Support Team,

I would like to confirm whether the Trimension NCJ29D6 UWB chip integrates both Secure Vehicle Access and In-Cabin Sensing capabilities, specifically Child Presence Detection (CPD), using the same hardware.
Is it correct to say that both functionalities can be supported simultaneously on the same NCJ29D6 chip, depending on the software configuration?

Thank you in advance for your clarification.


Reference:
https://embeddedhardwaredesign.com/nxp-unveils-first-monolithic-uwb-chip-ncj29d6-integrating-mcu-and...
The Trimension NCJ29D6 UWB chip, integrated into the car’s access system, can go beyond securing the vehicle. Through the same hardware, it enables child presence detection by sensing the UWB signals within the car’s interior. If the system detects the presence of a child after the parent has left the vehicle, it could trigger an alert or take preventive actions to ensure the child’s safety.

Thanks.
Best Regards,
Brian.

0 Kudos
Reply
2 Replies

2,944 Views
BrianYeh
Contributor I

OK.

thanks.

0 Kudos
Reply

3,008 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Sorry for the inconvenience this might cause you but as the information of this product it's under NDA (Non-Disclosure Agreement) the information it's not public.

 

For more information about the chip could you please contact one of our distributors available in the Distributor Network|NXP? Or if you have any direct contact, please contact them.

 

Regards,

Ricardo

0 Kudos
Reply