PE IIC component error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PE IIC component error

跳至解决方案
4,268 次查看
Ben
Senior Contributor I

Anyone know what is the problem with PE IIC component ? I am getting an error message while compiling PE code:

11565_11565.jpgI2C_error_Image.jpg

TIA

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
3,992 次查看
TICS_Fiona
NXP Employee
NXP Employee

To investigate the problem, I need to know the CodeWarrior version you are using, as well as the part number of your target MCU.

It will be greatly appreciated if you could attach a simple project to help us reproduce the error.

In addition, the latest version is v10.6, which can be downloaded from:

http://tinyurl.com/6jo5tge

The license for CW10.5 also work with CW 10.6.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,993 次查看
TICS_Fiona
NXP Employee
NXP Employee

To investigate the problem, I need to know the CodeWarrior version you are using, as well as the part number of your target MCU.

It will be greatly appreciated if you could attach a simple project to help us reproduce the error.

In addition, the latest version is v10.6, which can be downloaded from:

http://tinyurl.com/6jo5tge

The license for CW10.5 also work with CW 10.6.

0 项奖励
回复
3,992 次查看
Ben
Senior Contributor I

Fiona, as you asked for a simple project, it helped me in workaround this error. I created a new small project, and PW with I2C OK.

It is not the 1st time that I see that after freezing PE and writing long code, trying to reuse of the PE not always succeed.

Thank you, I understand that this is a bug, but consider my question solved. I copied the files from the new project I created to my application, and it works OK.

0 项奖励
回复
3,992 次查看
Ben
Senior Contributor I

Thanks Fiona for your fast response, CW10.6 & 56F8257

0 项奖励
回复