PE IIC component error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PE IIC component error

ソリューションへジャンプ
4,198件の閲覧回数
Ben
Senior Contributor I

Anyone know what is the problem with PE IIC component ? I am getting an error message while compiling PE code:

11565_11565.jpgI2C_error_Image.jpg

TIA

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
3,922件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

To investigate the problem, I need to know the CodeWarrior version you are using, as well as the part number of your target MCU.

It will be greatly appreciated if you could attach a simple project to help us reproduce the error.

In addition, the latest version is v10.6, which can be downloaded from:

http://tinyurl.com/6jo5tge

The license for CW10.5 also work with CW 10.6.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,923件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

To investigate the problem, I need to know the CodeWarrior version you are using, as well as the part number of your target MCU.

It will be greatly appreciated if you could attach a simple project to help us reproduce the error.

In addition, the latest version is v10.6, which can be downloaded from:

http://tinyurl.com/6jo5tge

The license for CW10.5 also work with CW 10.6.

0 件の賞賛
返信
3,922件の閲覧回数
Ben
Senior Contributor I

Fiona, as you asked for a simple project, it helped me in workaround this error. I created a new small project, and PW with I2C OK.

It is not the 1st time that I see that after freezing PE and writing long code, trying to reuse of the PE not always succeed.

Thank you, I understand that this is a bug, but consider my question solved. I copied the files from the new project I created to my application, and it works OK.

0 件の賞賛
返信
3,922件の閲覧回数
Ben
Senior Contributor I

Thanks Fiona for your fast response, CW10.6 & 56F8257

0 件の賞賛
返信