PE IIC component error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PE IIC component error

Jump to solution
4,215 Views
Ben
Senior Contributor I

Anyone know what is the problem with PE IIC component ? I am getting an error message while compiling PE code:

11565_11565.jpgI2C_error_Image.jpg

TIA

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
3,939 Views
TICS_Fiona
NXP Employee
NXP Employee

To investigate the problem, I need to know the CodeWarrior version you are using, as well as the part number of your target MCU.

It will be greatly appreciated if you could attach a simple project to help us reproduce the error.

In addition, the latest version is v10.6, which can be downloaded from:

http://tinyurl.com/6jo5tge

The license for CW10.5 also work with CW 10.6.

View solution in original post

0 Kudos
Reply
3 Replies
3,940 Views
TICS_Fiona
NXP Employee
NXP Employee

To investigate the problem, I need to know the CodeWarrior version you are using, as well as the part number of your target MCU.

It will be greatly appreciated if you could attach a simple project to help us reproduce the error.

In addition, the latest version is v10.6, which can be downloaded from:

http://tinyurl.com/6jo5tge

The license for CW10.5 also work with CW 10.6.

0 Kudos
Reply
3,939 Views
Ben
Senior Contributor I

Fiona, as you asked for a simple project, it helped me in workaround this error. I created a new small project, and PW with I2C OK.

It is not the 1st time that I see that after freezing PE and writing long code, trying to reuse of the PE not always succeed.

Thank you, I understand that this is a bug, but consider my question solved. I copied the files from the new project I created to my application, and it works OK.

0 Kudos
Reply
3,939 Views
Ben
Senior Contributor I

Thanks Fiona for your fast response, CW10.6 & 56F8257

0 Kudos
Reply