MC56F844x dflash programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC56F844x dflash programming

Jump to solution
2,924 Views
jolantamienkino
Contributor II

Hello,

using MC56F844789. This device has Primary program/data flash memory, mapped into 0x00 0000 - 0x01 ffff & 0x02 0000 - 0x03 ffff, and also Secondary (boot) program/data flash memory, mapped into 0x06 8000 - 0x06 bfff & 0x00 8000 - 0x00 bfff. 

I can program Primary program/data flash memory, when only providing flash command an address within program space range (0x00 0000 - 0x01 ffff) - programing / erasing doesn't work when providing address from aliased data space.

However, I cannot program Secondary (boot) program/data flash memory regardless if flash command is given an address from program or data space. Software has been uploaded with checkbox "always mass erase on download" and therefore data flash shall default to 32 Kbytes of data flash, No EEPROM.

Can you please advise how to program Secondary (boot) program/data flash memory from within user application?

Thanks,

Jolanta.

0 Kudos
Reply
1 Solution
2,800 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jolanta,

Regarding the address generation, as you know that the Flash of MC56F84xxx/MC56F82xxx use the flash IP which is the same as Kinetis, the flash IP use Byte(8 bits) accessing mode, the MC56F84xxx/82xxx use half word address mode(16 bits), so the address is left shifted by ONE bit. There are program Flash and Data Flash for DSC, they are in different domain, so we use bit23 to identify the program/data flash type. But all the information are not documented in DSC reference manual.  I am sorry for the inconvenience.

BR

Xiangjun Rong

View solution in original post

4 Replies
2,799 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jolanta Mienkinova

I forgot to attach the example, here, I attach it.

BR

Xiangjun Rong

2,799 Views
jolantamienkino
Contributor II

Hi Rong,

thanks for example. It works after address of data flash to be programmed /erased is pre-processed:

*((dword *)(void *)&FTFL_FCCOB3) = (dword)(((Address - DATA_FLASH_START) << 1) | (1UL << 23));

I couldn't find this key information about address pre-processing in device reference manual. If there is such a section, and I just didn't notice it, please provide reference. 

Thanks,

Jolanta.

0 Kudos
Reply
2,801 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jolanta,

Regarding the address generation, as you know that the Flash of MC56F84xxx/MC56F82xxx use the flash IP which is the same as Kinetis, the flash IP use Byte(8 bits) accessing mode, the MC56F84xxx/82xxx use half word address mode(16 bits), so the address is left shifted by ONE bit. There are program Flash and Data Flash for DSC, they are in different domain, so we use bit23 to identify the program/data flash type. But all the information are not documented in DSC reference manual.  I am sorry for the inconvenience.

BR

Xiangjun Rong

2,799 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jolanta,

Regarding your question, we have the processor Expert(PE), the PE has intFLASH bean, with which you can erase both Program/data Flash, program Program/Data Flash.

This is the bean:

pastedImage_1.png

In the IntFLASH bean, you can select data Flash as Following:

pastedImage_2.png

I attach an example for MC56F84789  which is based on CodeWarrior for mcu ver11 tools can erase/program program flash, it tell you how to call the erasing function and program function. You can select the data flash and program it based on the erase/program function with different address and size.

Hope it can help you

BR

Xiangjun rong

0 Kudos
Reply