MC56F82748 clock configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F82748 clock configuration

ソリューションへジャンプ
2,093件の閲覧回数
terrybogard
Contributor II

dear nxp expert,

when I use processor expert to configure clock of MC56F82748, I set Clock configurations as 2, then come out configuration 0 and configuration 1. so what's the difference between 0 and 1? and why this can be set as 2, I found most demo project is 1.

 

terrybogard_0-1616558433865.png

 

0 件の賞賛
返信
1 解決策
2,080件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

H, Cai,

Pls refer to the screenshot, if you add more clock configuration, the PE will generate more clock configuration, you can call the CPU_SetClockConfiguration(LDD_TClockConfiguration ModeID) to select one.

Hope it can help you

BR

Xiangjun Rong

xiangjun_rong_0-1616574359178.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,081件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

H, Cai,

Pls refer to the screenshot, if you add more clock configuration, the PE will generate more clock configuration, you can call the CPU_SetClockConfiguration(LDD_TClockConfiguration ModeID) to select one.

Hope it can help you

BR

Xiangjun Rong

xiangjun_rong_0-1616574359178.png

 

0 件の賞賛
返信