MC56F82748 clock configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC56F82748 clock configuration

Jump to solution
2,119 Views
terrybogard
Contributor II

dear nxp expert,

when I use processor expert to configure clock of MC56F82748, I set Clock configurations as 2, then come out configuration 0 and configuration 1. so what's the difference between 0 and 1? and why this can be set as 2, I found most demo project is 1.

 

terrybogard_0-1616558433865.png

 

0 Kudos
Reply
1 Solution
2,106 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

H, Cai,

Pls refer to the screenshot, if you add more clock configuration, the PE will generate more clock configuration, you can call the CPU_SetClockConfiguration(LDD_TClockConfiguration ModeID) to select one.

Hope it can help you

BR

Xiangjun Rong

xiangjun_rong_0-1616574359178.png

 

View solution in original post

0 Kudos
Reply
1 Reply
2,107 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

H, Cai,

Pls refer to the screenshot, if you add more clock configuration, the PE will generate more clock configuration, you can call the CPU_SetClockConfiguration(LDD_TClockConfiguration ModeID) to select one.

Hope it can help you

BR

Xiangjun Rong

xiangjun_rong_0-1616574359178.png

 

0 Kudos
Reply