MC56F82748 I2C pull up resistor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC56F82748 I2C pull up resistor

1,622 次查看
EngHuiPeng
NXP Employee
NXP Employee

Is there any recommended pull up resistor for SCL and SDA lines of the I2C peripherals. This is for MC56F82748(Anguilla Silver)

标签 (1)
0 项奖励
回复
2 回复数

1,364 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, HuiPeng,

I think 4.7K ohm pull-up resistor is okay for the open drain IIC pins: SCL/SDA for MC56F82xxx.

BR

Xiangjun Rong

0 项奖励
回复

1,364 次查看
Stano
NXP Employee
NXP Employee

Hi HuiPeng,

for the 400pF max capacitance and 100kHz max communication speed the max pull-up resistor is 4k7. I suggest you to use 2k7 or 3k3 as pull-ups.

BR,

Stano.

0 项奖励
回复