MC56F82748 I2C pull up resistor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC56F82748 I2C pull up resistor

2,024 Views
EngHuiPeng
NXP Employee
NXP Employee

Is there any recommended pull up resistor for SCL and SDA lines of the I2C peripherals. This is for MC56F82748(Anguilla Silver)

Labels (1)
0 Kudos
Reply
2 Replies

1,766 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, HuiPeng,

I think 4.7K ohm pull-up resistor is okay for the open drain IIC pins: SCL/SDA for MC56F82xxx.

BR

Xiangjun Rong

0 Kudos
Reply

1,766 Views
Stano
NXP Employee
NXP Employee

Hi HuiPeng,

for the 400pF max capacitance and 100kHz max communication speed the max pull-up resistor is 4k7. I suggest you to use 2k7 or 3k3 as pull-ups.

BR,

Stano.

0 Kudos
Reply