MC56F82748 I2C pull up resistor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F82748 I2C pull up resistor

1,557件の閲覧回数
EngHuiPeng
NXP Employee
NXP Employee

Is there any recommended pull up resistor for SCL and SDA lines of the I2C peripherals. This is for MC56F82748(Anguilla Silver)

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,299件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, HuiPeng,

I think 4.7K ohm pull-up resistor is okay for the open drain IIC pins: SCL/SDA for MC56F82xxx.

BR

Xiangjun Rong

0 件の賞賛
返信

1,299件の閲覧回数
Stano
NXP Employee
NXP Employee

Hi HuiPeng,

for the 400pF max capacitance and 100kHz max communication speed the max pull-up resistor is 4k7. I suggest you to use 2k7 or 3k3 as pull-ups.

BR,

Stano.

0 件の賞賛
返信