Clock generation in CAN bus devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clock generation in CAN bus devices

Jump to solution
4,995 Views
rknispel
Contributor II

I am looking for details of the clock generation in UJA1169ATK/F:

  • clock source
  • PLL
  • Jitter in 13 bit interval of CAN communications

Is there a technology papaer where it can be derived from?

0 Kudos
Reply
1 Solution
4,925 Views
rknispel
Contributor II

The question was transferred into a service case and resolved there.

View solution in original post

0 Kudos
Reply
6 Replies
4,926 Views
rknispel
Contributor II

The question was transferred into a service case and resolved there.

0 Kudos
Reply
4,976 Views
guoweisun
NXP TechSupport
NXP TechSupport

What kinds of clock detail information do you need?

0 Kudos
Reply
4,974 Views
rknispel
Contributor II

My questionnaire is about details of the Automotive qualification of the CAN communications of UJA1169ATK/F:

CAN network clock source
PLL frequency [MHz]
max. PLL jitter in 13 bit interval
oscillator manufacturer
oscillator part name
oscillator frequency [MHz]
oscillator tolerance [%]

Possible answers include clock recovery from CANH/CANL lines, and the oscillator would be MCU oscillator.

0 Kudos
Reply
4,956 Views
guoweisun
NXP TechSupport
NXP TechSupport

These parameters should be checked or setting in CAN controller side,right?UJA1169 is CAN transceiver.

4,950 Views
rknispel
Contributor II

The parameters are relevant for reliabilty of CAN communications in on-board network as Automotive application. UJA1169 is considered for SBC of such a component.

Typically the internal clock is generated from TXD by clock recovery. I am looking for more details on this process!

Help is very much appreciated and thanks for any hints in advance!

0 Kudos
Reply
4,990 Views
rknispel
Contributor II

The data sheet says "microcontrollerindependent clock source" is present on the chip, but where can further details be taken from?

0 Kudos
Reply