Clock generation in CAN bus devices

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clock generation in CAN bus devices

ソリューションへジャンプ
4,690件の閲覧回数
rknispel
Contributor II

I am looking for details of the clock generation in UJA1169ATK/F:

  • clock source
  • PLL
  • Jitter in 13 bit interval of CAN communications

Is there a technology papaer where it can be derived from?

0 件の賞賛
返信
1 解決策
4,620件の閲覧回数
rknispel
Contributor II

The question was transferred into a service case and resolved there.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
4,621件の閲覧回数
rknispel
Contributor II

The question was transferred into a service case and resolved there.

0 件の賞賛
返信
4,671件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

What kinds of clock detail information do you need?

0 件の賞賛
返信
4,669件の閲覧回数
rknispel
Contributor II

My questionnaire is about details of the Automotive qualification of the CAN communications of UJA1169ATK/F:

CAN network clock source
PLL frequency [MHz]
max. PLL jitter in 13 bit interval
oscillator manufacturer
oscillator part name
oscillator frequency [MHz]
oscillator tolerance [%]

Possible answers include clock recovery from CANH/CANL lines, and the oscillator would be MCU oscillator.

0 件の賞賛
返信
4,651件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

These parameters should be checked or setting in CAN controller side,right?UJA1169 is CAN transceiver.

4,645件の閲覧回数
rknispel
Contributor II

The parameters are relevant for reliabilty of CAN communications in on-board network as Automotive application. UJA1169 is considered for SBC of such a component.

Typically the internal clock is generated from TXD by clock recovery. I am looking for more details on this process!

Help is very much appreciated and thanks for any hints in advance!

0 件の賞賛
返信
4,685件の閲覧回数
rknispel
Contributor II

The data sheet says "microcontrollerindependent clock source" is present on the chip, but where can further details be taken from?

0 件の賞賛
返信