uTasker 1.4 Unknown USB device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uTasker 1.4 Unknown USB device

4,010件の閲覧回数
ing_albertopc
Contributor I

Hi !

I'm using the uTasker 1.4 for kinetis on a custom board. I followed the steps on this post uTasker Bootloader Porting Guide ,I loaded the bin file and the board goes on bootloader mode but when i connect the USB to a computer it says Unknown device.

I'm using a MK53DN512 and a TWR-K53N512 configuration.

Is this a problem with the driver?

How can i solve this?

I'll be thanckful for your help.

Regards.

Alberto Peña

Original Attachment has been moved to: uTaskerKinetisV1.4.7.rar

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,576件の閲覧回数
ing_albertopc
Contributor I

Finally i solved it, was a problem with the USB clock.

Now when i try to send the file, the bootloader answer  "BAD FORMAT", I followed the steps on this post How to create .s19 file from project settings to get the s19 file from the application proyect.

I'll be thankful for your help.

Regards

0 件の賞賛
返信

3,576件の閲覧回数
mjbcswitzerland
Specialist V

Hi

I have just seen this - 3 years too late.

If it has been posted in the Kinetis forum I would have answered immediately. Sorry...

Regards

Mark

Complete Kinetis solutions for professionals, training and support: http://www.utasker.com/kinetis.html

0 件の賞賛
返信

3,576件の閲覧回数
TomE
Specialist II

If you don't get an answer here I'd suggest you look on the uTasker site.

Read documents like this one (that detail the driver you have to install on your PC to get this to work) or read the Forums there:

http://www.utasker.com/docs/uTasker/uTaskerV1.3_USB_Demo.PDF

Tom

0 件の賞賛
返信

3,576件の閲覧回数
ing_albertopc
Contributor I

Hi!

Thanks for your answer Tom, i have looked into the uTasker forum and found some post that help a little but still don't get any luck, i don't know what else to do.

0 件の賞賛
返信