uTasker 1.4 Unknown USB device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uTasker 1.4 Unknown USB device

3,976 Views
ing_albertopc
Contributor I

Hi !

I'm using the uTasker 1.4 for kinetis on a custom board. I followed the steps on this post uTasker Bootloader Porting Guide ,I loaded the bin file and the board goes on bootloader mode but when i connect the USB to a computer it says Unknown device.

I'm using a MK53DN512 and a TWR-K53N512 configuration.

Is this a problem with the driver?

How can i solve this?

I'll be thanckful for your help.

Regards.

Alberto Peña

Original Attachment has been moved to: uTaskerKinetisV1.4.7.rar

Labels (1)
0 Kudos
Reply
4 Replies

3,542 Views
ing_albertopc
Contributor I

Finally i solved it, was a problem with the USB clock.

Now when i try to send the file, the bootloader answer  "BAD FORMAT", I followed the steps on this post How to create .s19 file from project settings to get the s19 file from the application proyect.

I'll be thankful for your help.

Regards

0 Kudos
Reply

3,542 Views
mjbcswitzerland
Specialist V

Hi

I have just seen this - 3 years too late.

If it has been posted in the Kinetis forum I would have answered immediately. Sorry...

Regards

Mark

Complete Kinetis solutions for professionals, training and support: http://www.utasker.com/kinetis.html

0 Kudos
Reply

3,542 Views
TomE
Specialist II

If you don't get an answer here I'd suggest you look on the uTasker site.

Read documents like this one (that detail the driver you have to install on your PC to get this to work) or read the Forums there:

http://www.utasker.com/docs/uTasker/uTaskerV1.3_USB_Demo.PDF

Tom

0 Kudos
Reply

3,542 Views
ing_albertopc
Contributor I

Hi!

Thanks for your answer Tom, i have looked into the uTasker forum and found some post that help a little but still don't get any luck, i don't know what else to do.

0 Kudos
Reply