problem aboutMCF52211's RTC module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

problem aboutMCF52211's RTC module

跳至解决方案
2,157 次查看
bluehacker
Contributor III
I want to use mcf52211 to develop one product. I want to use its RTC module,but I hope it can keep running even when VDD,VDDPLL is power down, the mcf52211 has VSTBY pin,so I think use a battery backup power to VSTBY pin. my question is whether the method works?
thanks!
标签 (1)
0 项奖励
回复
1 解答
1,516 次查看
mjbcswitzerland
Specialist V
Hi

The RTC can be used together with 32kHz crystal and battery backup.

See also http://www.utasker.com/forum/index.php?topic=256.0

Note that the 32kHz crystal shares pins with UART0, meaning that UART0 can no longer be used if the RTC crystal is required. This restriction is removed in the M5225X family, where there are dedicated 32kHz RTC crystal inputs.

Regards

Mark


www.uTasker.com



在原帖中查看解决方案

0 项奖励
回复
1 回复
1,517 次查看
mjbcswitzerland
Specialist V
Hi

The RTC can be used together with 32kHz crystal and battery backup.

See also http://www.utasker.com/forum/index.php?topic=256.0

Note that the 32kHz crystal shares pins with UART0, meaning that UART0 can no longer be used if the RTC crystal is required. This restriction is removed in the M5225X family, where there are dedicated 32kHz RTC crystal inputs.

Regards

Mark


www.uTasker.com



0 项奖励
回复