problem aboutMCF52211's RTC module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem aboutMCF52211's RTC module

Jump to solution
2,158 Views
bluehacker
Contributor III
I want to use mcf52211 to develop one product. I want to use its RTC module,but I hope it can keep running even when VDD,VDDPLL is power down, the mcf52211 has VSTBY pin,so I think use a battery backup power to VSTBY pin. my question is whether the method works?
thanks!
Labels (1)
0 Kudos
Reply
1 Solution
1,517 Views
mjbcswitzerland
Specialist V
Hi

The RTC can be used together with 32kHz crystal and battery backup.

See also http://www.utasker.com/forum/index.php?topic=256.0

Note that the 32kHz crystal shares pins with UART0, meaning that UART0 can no longer be used if the RTC crystal is required. This restriction is removed in the M5225X family, where there are dedicated 32kHz RTC crystal inputs.

Regards

Mark


www.uTasker.com



View solution in original post

0 Kudos
Reply
1 Reply
1,518 Views
mjbcswitzerland
Specialist V
Hi

The RTC can be used together with 32kHz crystal and battery backup.

See also http://www.utasker.com/forum/index.php?topic=256.0

Note that the 32kHz crystal shares pins with UART0, meaning that UART0 can no longer be used if the RTC crystal is required. This restriction is removed in the M5225X family, where there are dedicated 32kHz RTC crystal inputs.

Regards

Mark


www.uTasker.com



0 Kudos
Reply